I would like to ask, where to choose the 1Tx launch and 2Tx launch settings for iwr1642 using mmwave studio. I tried to change the check box of the option box under chirp in the figure below (others use the default parameters). Channel, under the same conditions of other parameters, check Tx0 and Tx0Tx1 at the same time, there is no difference in the file size. If I choose one transmission channel and two transmission channels, it is wrong:
1. Please tell me how do I choose one or two transmission channels?
If there are no errors:
2. Does this mean that the number of transmission channels does not affect the file size?
last question:
3. What effect will the number of transmitting channels have?
Looking forward to your answer