我想找一款3.0V-4.5V输入,升压到5.0V,输出电流大于150mA,纹波要小的升压芯片,类似TPS61071DDC这款芯片,但要比这款芯片的纹波还要小,请问有什么推荐的型号吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想找一款3.0V-4.5V输入,升压到5.0V,输出电流大于150mA,纹波要小的升压芯片,类似TPS61071DDC这款芯片,但要比这款芯片的纹波还要小,请问有什么推荐的型号吗?
您好!
要减小输出电压纹波,一个方法是增大电感和电容,另一个方法是提高开关频率。
我在TI的WEBENCH设计工具上为您简单选了一下,电感10uH,电容10uF时,TPS61071的输出纹波为5.758mV。
我为您推荐LM2731X,相同电感和电容下,输出纹波仅为1mV左右。
不知道您对于成本有没有要求?如果需要,请email我nison-wang@ti.com,我可以为您分析一下成本。
你好,
这颗芯片的频率1,2Mhz,相对较高,你可以考虑增加输出电容实现,增加电感效果不明显,谢谢。
给你看一篇文章,选择合适的就好,不要一味地追求性能。