芯片EN脚悬空或下拉5.1K至GND时,芯片无法关闭,一直有微弱的不稳定的电压输出大致在3~4V之间。可能是什么原因?
输入为3V1A电源,正常输出5V0.2A
P1_12 3V输入 P1_34 GND P3是一个船型开关接口 C20 100uF C22 C23 220uF C6 C7 10uF 10V钽电容 L1 6.8uH 4.8A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
芯片EN脚悬空或下拉5.1K至GND时,芯片无法关闭,一直有微弱的不稳定的电压输出大致在3~4V之间。可能是什么原因?
输入为3V1A电源,正常输出5V0.2A
P1_12 3V输入 P1_34 GND P3是一个船型开关接口 C20 100uF C22 C23 220uF C6 C7 10uF 10V钽电容 L1 6.8uH 4.8A
后级是一个ldo带一块avr和运放 其他的都断开了
我用io接了一个led 然后程序开始时点亮 发现led是闪烁的 用示波器看tps61032的输出完全是乱跳的