用LM5140-Q1驱动GaN时,VCC 脚失效,具体情况是:在工作一段时间后,vcc突然降到0V,经测量,16pin到地阻抗很低,有的接近为0,15pin阻抗正常;15pin和16pin在PCB板上都是VCC,由LM5140-Q1芯片内部LDO出来的;同样是VCC电源网络,16pin被打坏,15pin是好的,3块板子同样的情况,不知道这种情况是怎么引起的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用LM5140-Q1驱动GaN时,VCC 脚失效,具体情况是:在工作一段时间后,vcc突然降到0V,经测量,16pin到地阻抗很低,有的接近为0,15pin阻抗正常;15pin和16pin在PCB板上都是VCC,由LM5140-Q1芯片内部LDO出来的;同样是VCC电源网络,16pin被打坏,15pin是好的,3块板子同样的情况,不知道这种情况是怎么引起的。
推测还是和MOS有关,能换成硅片MOS试一下么
或者你抓取一下MOS的驱动波形,上传一下