hi:
我使用你们家的BQ25890+BQ25892双芯片充电时,两颗芯片的温度在充电过程中(半个小时左右)会达到70℃,此时输入端的功率约为12V/1.4A,流入电池端的电流约为4A。这个温度与你们官方说明半小时约50度差距很大,请问我这个温度是正常的吗?是否是因为电路的设计问题导致发热过大?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
20℃对于一般电源芯片而言影响不大,但是在电池充电中或要引起注意,看这个对于芯片温度sense侦测影响是否比较大?
对于差异,主要在于layout, 对于内置MOS的功率转换,要特别注意layout , Powerpad连接的GND面积,是否利用四层板中间GND层散热等影响都很大。具体你可以看看TI的评估版。