This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想问下TI的工作人员,TPS54160和TPS54160A有什么区别呢
楼主可以参考一下datasheet
Hi
其次就是TPS54160A有2中封装模式,而TPS54160只有一种, 如上表。
以及人体ESD模式TPS54160A是2kV, 而TPS54160只有1kV.
不是特别清楚UVLO的影响. 请问一下, 24V~48V转5V 200mA的应用中, 使用TPS54160ADGQR替换TPS54160DGQR, 需要注意哪些问题呢? 是否可以直接替换使用. 谢谢!
可以直接替换