Other Parts Discussed in Thread: TPS61070
我的TPS61070在空载时输入1V输出5.20V(空载时) 然后输入上升时输出也上升没有稳在5V。为什么? 所有参数都跟原理图一样 就把最后那两个电阻换为100K 和940K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输出电容需足够,推荐是2个4.7uF的低ESR 陶瓷电容(0603尺寸,或者可以增加到3个),尽量靠近芯片Vout脚。
请问您的测试是在空载还是有载(多大载)状态下?
包括分压电阻,电感,输入输出电容都要尽量靠近芯片。
另外之前提到的电阻,180k/1600k是datasheet推荐,而事实上100k/940k也是没有问题的,设计要求是R2(低边电阻)是要求在200k欧姆以下,而FB分压电阻越大,此电阻功耗也就越小,所以选的180kohm.
请问空载下50Hz的锯齿波幅值是多少? 有负载时此幅值又是多大? 最好是能提供相应的波形给我,并说明对应负载是多少?