Other Parts Discussed in Thread: LM3478, LM5022, LM5176
LM3478输出空载,输入电源小于4A时,LM3478的6脚DR脚会一直输出高电平,导致mos短路,前级过流保护不起效(占空比为1的坏处);我自己手动在LM3478的Vin脚增加一个开关,待pcb上电后,我在开启Vin,这样输入的启动电流很小都不会短路,麻烦TI的员工给分析一下是否有什么软开关的电路,或者在芯片周围参数做处理,就能解决。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
这个不是bug, 应该是芯片电路或者电感没有设计好, 建议你按照下面这个文档,重新确认一下电路的参数或者相关器件的规格。
http://www.ti.com.cn/cn/lit/an/zhca228/zhca228.pdf
你好,电源电路已经按照ti生成器生成,而且,如果是电路设计不好,为啥我手动给芯片的Vin延后上电就可以???已经询问过ti相关技术人员,这个芯片就是存在这样的问题;麻烦请教一下你,LM5022是否也可以使用这样的升降压电路???
输入电压9V-40V,请教一下你是否LM5022可以使用类似LM3487的电路???
目前可以确认的现象,把输入电容调小一些,这样开机瞬态电流可以小一些(也就是说原来要大于等于4A才不会短路,现在3A以上都不会短路了);还有就是断开芯片的Vin,等到电解电容都上电后,手动上电就不存在短路现象;目前分析是因为LM3478的VCC大于3V即可工作,而且占空比可以达到1,这样导致,如果前级电容上电的时间稍微长一些,芯片在3V工作,这个时候输出电压12V达不到,芯片增加占空到1,导致电感mos不震荡,mos直接短路,芯片的短路保护功能丧失!!!!
遇到同样的问题了,并且也是Vin后上电才能有输出,请问这个问题有什么办法能解决,毕竟不能总是手工来控制