现在情况是我的10.4v电压输出正常,-7v电压达到了-9v,16V电压达到了18V,我想请教一下为什么会出现这种情况,这种情况出现的原因是什么呢?我的电路肯定没问题,因为这是一批板子,这块焊接出来就不行,而且带上同样的负载=9v变成-13v,18v却上升为21v,但是10.4v正常,这是什么原因呢?这个电路怎么计算的到的这些电压,手册上只是说10.4v是1.233*(1+R1/R2),想知道原因,求给讲解一下!万分感谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
-7V这边是反向chargepump, 也就是10.4V反向得到-10.4V, 然后通过稳压管,得到7V左右。
16V这边是正常倍压chargepump, 也就是10.4V倍压得到20.8V, 然后通过稳压管得到16V左右。