Other Parts Discussed in Thread: TPS56221
如题,按照datasheet搭建电路,按照设计,TPS56221输出电压为1.0V,但是实际输出为0.52V
输入电压5V,VDD=5V
经测试,pin2 V(fb)=0.32V,与datasheet描述不符V(fb)=0.6V
经测试,V(bp)=5V,与datasheet描述不符V(bp)=6.5V
使能端pin21由NMOSFET控制,悬空后,测得pin21电压为4.01V
请大侠指点,多谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.