TPS70933的输入范围很宽,输出电压固定为3.3V,输出电流最大150mA。我现在设计电源,可以选择直接将主电源9.5V直接接到TPS70933的输入端,也可以选择将主电源经过DCDC TLV62130降压到3.7V左右后,在接到TPS70933的输入端。我想查一下TPS70933输出固定为3.3V150mA的情况下,输入电压分别为9.5V和3.7V时,TPS70933的效率分别是多少?我在datasheet上没有查到,可否帮忙支持一下,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.