您好,
我们现在使用了TPS61032芯片做设计,输入电源采用两节AA电池。想把3V 输入电压BOOST 到5V, 然后给后面的MPM3810芯片使用。 现在只要一接入电池测量VIN处电压就变成2V左右,然后TPS61032的输出电压一直是3V左右。麻烦帮我们看一下这个设计是否有误。我们原理图中的D2没有用。麻烦请问这里是否需要加入RC电路?
Vin=2V; VBAT_O=1.8~1.9V; Vout=3.14V
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我们现在使用了TPS61032芯片做设计,输入电源采用两节AA电池。想把3V 输入电压BOOST 到5V, 然后给后面的MPM3810芯片使用。 现在只要一接入电池测量VIN处电压就变成2V左右,然后TPS61032的输出电压一直是3V左右。麻烦帮我们看一下这个设计是否有误。我们原理图中的D2没有用。麻烦请问这里是否需要加入RC电路?
Vin=2V; VBAT_O=1.8~1.9V; Vout=3.14V
非常感谢!