客户拿到了USB2ANY工具,帮助客户将23880demo连接上PC端,可以通过软件看到当前Demo板的状态: 2-4Pair ports & 4-2 Pair ports
进入工程界面可以看到端口的状态显示为75W,也是默认配置的状态 Req:Class8 Assign:Class6,但是客户的需求是 Req:Class8 Assign:Class8才能达到90W的功率,调试过程中,通过Register Map界面进行设置,想通过设置0X29寄存器4PWnn设置为1 MCnn_2-0 为111后让功率变为90W,但是在写寄存器后,如果重新读取,寄存器的值会恢复默认, 当前MCnn_2-0默认的是110,写入111后读取还是110,从而功率无法变为90W。能否提供设置的步骤,非常感谢。