电路是典型电路,电感是10uH,检测电流电阻是10毫欧,调试用的是可调数字电源,当限流为10A以下时,无法启动,输出占空比为100%,电源处于CC模式,电压下降。感觉这个芯片上电瞬间要达到过流保护值,才能够正常启动,空载启动就要10A以上的电流
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电路是典型电路,电感是10uH,检测电流电阻是10毫欧,调试用的是可调数字电源,当限流为10A以下时,无法启动,输出占空比为100%,电源处于CC模式,电压下降。感觉这个芯片上电瞬间要达到过流保护值,才能够正常启动,空载启动就要10A以上的电流
LM3488空载上电电流非常大的问题,在LM3488的SEPIC电路中同样现象,问题后来解决了。
上电时,LM3488的DR脚输出给MOSFET栅极的PWM信号电压不足3V,并缓慢上升,当电压达到MOSFET的Vgs时,MOSFET开始打开。这就需要MOSFET的Vgs的阈值小于3V,最好在2.8V左右。如果MOSFET的Vgs大于3V,将会有一段缓慢的电压上升时间,此时间段内,输入端电流非常大,具体原因不明。WEBENCH中SEPIC电路推荐的CSD19538的Vgs阈值在4V以上,不能满足LM3488,后来更换了Vgs低于3V的MOSFET,上电电流问题解决了。图片是上电时,栅极电压。
感谢回答我的问题,后面我换个低启动电压的mos试试看。这些问题,手册里面都没有提到过,感觉就是个坑,电流斜坡补偿好像也有点问题。