This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

24V输入,9-36V输出,电流500mA,求教电源设计方案...

Other Parts Discussed in Thread: LM2596, LM358, LM2585

大家好,

最近有手头有个项目,中间要用到输出可调的电源。

具体情况如下:系统是24VDC输入,要求输出9-36VDC可调,电流很小,500mA就足够。

现在系统里面有一个MSP430的控制器,一直想不到很好的解决方案,所以来请教一下。因为产品里面的空间非常有限,对体积有一定要求。


目前我有的思路是分两步:

1.先用DC-DC来升压,升到一个固定的电压,24VDC升压到36V+1.7VDC(LM2596调压是需要电压差);

2.采用2596-ADJ+LM358+MSP430来实现电压可调,最终达到9-36V输出的结果。

目前想到的就是这个方案。因为之前没做过电源,只是看过一些资料。

不知道还有没有其他更好的方案?

非常感谢