This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS54062上电开关频率的问题

TPS54032作同步buck降压用途,设计24V转15V输出40mA电流。芯片为峰值电流PWM控制型。

我采用100uH电感、10uF输出电容和400K开关频率。测试中使用直流电阻负载,发现输出电流由20mA上升到40mA时电流可以稳定工作,但是直接40mA上电时,输出电压就几V了。继续测试发现,27mA左右得输出电流为极限,此时上电后电感峰值电流为86mA,远未到达120mA的电流限制。再增加输出电流,上电后电压又只有几V。

经过进一步测试发现,正常上电时,开关频率从50k、100K、200K、400K(此时电感峰值电流都达到120mA)软启动。但是当我输出电流大于27mA时,启动的开关频率跑到100K,电压就不爬升了,频率也不提高了。

综上,在400K可以稳定输出40mA的电路。由于软启动开关频率停留在100k导致输出异常。请问除了提高电感量之外还有其他解决方法吗。或者说具体解释下上电时这个频率切换的具体机制(稳定运行时CCM模式达到峰值电流似乎就会分频降频),谢谢了。