【电子书下载】- 《电源设计经验谈》

本书下载地址:http://www.ti.com/cn/lit/pdf/ZHCC344

作者介绍:
Robert Kollman 现任 TI 高级应用经理兼科技委员会的资深委员。他拥有在电源电子领域超过 30 年的工作经验,并为电源电子设计了从低功耗 (sub-watt)到超低功耗 (sub-megawatt) 的磁性元件,工作频率在兆赫兹范围内。Robert 毕业于得克萨斯 A&M 大学 (Texas A&MUniversity) , 获电子工程理学士学位, 后又毕业于南卫理公会大学(Southern Methodist University),获电子工程硕士学位。

目录

电源设计经验谈1:为您的电源选择正确的工作频率 ......................................................................................... 5
电源设计经验谈2:驾驭噪声电源 ........................................................................................................................ 6
电源设计经验谈3:阻尼输入滤波器——第一部分............................................................................................. 8
电源设计经验谈4:阻尼输入滤波器系列之第二部分 ....................................................................................... 10
电源设计经验谈5:降压—升压电源设计中降压控制器的使用 ....................................................................... 11
电源设计经验谈6:精确测量电源纹波 ................................................................................................................13
电源设计经验谈7:高效驱动 LED 离线式照明 ................................................................................................. 14
电源设计经验谈8:通过改变电源频率来降低 EMI 性能 .................................................................................. 16
电源设计经验谈9:估算表面贴装半导体的温升 ............................................................................................... 18
电源设计经验谈10:轻松估计负载瞬态响应 ..................................................................................................... 20
电源设计经验谈11:解决电源电路损耗问题 ..................................................................................................... 21
电源设计经验谈12:电源效率最大化 ................................................................................................................. 22
电源设计经验谈13:小心别被电感磁芯损耗烫伤 ............................................................................................. 24
电源设计经验谈14:SEPIC 转换器提供高效偏置电源 .................................................................................... 25
电源设计经验谈15:低成本、高性能 LED 驱动器 ........................................................................................... 27
电源设计经验谈16:缓冲正向转换器 ................................................................................................................. 29
电源设计经验谈17:缓冲反向转换器 ................................................................................................................. 33
电源设计经验谈18:您稳压器的输出电压精度或许并非如您所想的那样糟糕 ............................................. 35
电源设计经验谈19:轻松创建多个负输出电压 ................................................................................................. 38
电源设计经验谈20:注意那些意外谐振响应 ..................................................................................................... 40
电源设计经验谈21:请注意电容 RMS 纹波额定电流! .................................................................................. 42
电源设计经验谈22:避免一些常见的误差放大器使用错误 ............................................................................. 44
电源设计经验谈23:改善负载瞬态响应 ............................................................................................................. 46
电源设计经验谈24:并-串联阻抗转换 ................................................................................................................ 47
电源设计经验谈25:改善负载瞬态响应—第 2 部分 ......................................................................................... 50
电源设计经验谈26:高频导体的电流分布 ......................................................................................................... 52
POWER TIP 27: PARALLELING POWER SUPPLIES USING THE DROOP METHOD ............................ 54

电源设计经验谈 28:估算热插拔 MOSFET 的瞬态温升——第 1 部分 ......................................................... 56
电源设计经验谈 29:估算热插拔 MOSFET 的瞬态温升——第 2 部分 ......................................................... 57
电源设计经验谈 30:低压降压 IC 让简捷、经济的偏置电源成为现实 ......................................................... 59
电源设计经验谈 31:同步降压 MOSFET 电阻比的正确选择 ......................................................................... 61
电源设计经验谈 32:注意 SEPIC 耦合电感回路电流—第 1 部分 ................................................................. 62
电源设计经验谈 33:注意 SEPIC 耦合电感回路电流——第2 部分 .............................................................. 64
电源设计经验谈 34:设计简易的隔离式偏压电源 ........................................................................................... 66
POWER TIP 35: MINIMIZE TRANSFORMER INTERWINDING CAPACITANCE ........................................ 68
电源设计经验谈 36:使用高压 LED 提高灯泡效率 .......................................................................................... 71
电源设计经验谈 37:折中选择输入电容纹波电流的线压范围 ........................................................................ 73
电源设计经验谈38:使用简易锁存电路保护电源 ............................................................................................. 75
电源设计经验谈 39:同步整流带来的不仅仅是高效率 .................................................................................... 77
电源设计经验谈 40:非隔离式电源的共模电流 ................................................................................................ 78
电源设计经验谈 41:DDR 内存电源 .................................................................................................................. 80
电源设计经验谈 42:可替代集成 MOSFET 的分立器件 .................................................................................. 82
电源设计经验谈 43:分立器件——一款可替代集成 MOSFET 驱动器的卓越解决方案 .............................. 84
电源设计经验谈 44:如何处理高 DI/DT 负载瞬态 ............................................................................................ 85
电源设计经验谈 45:如何处理高DI/DT 负载瞬态(下) ...................................................................................... 87
电源设计经验谈 46:正确的同步降压 FET 时序 ............................................................................................... 90
电源设计经验谈 47:解决隔离式开关的传导性共模辐射问题 ........................................................................ 92
电源设计经验谈 48:解决隔离式开关的传导性共模辐射问题之第 2 部分 .................................................... 93
电源设计经验谈 49:多层陶瓷电容器常见小缺陷的规避方法 ........................................................................ 95
电源设计小贴士 50:铝电解电容器常见缺陷的规避方法 ................................................................................ 97

 

本书下载地址:http://www.ti.com/cn/lit/pdf/ZHCC344

 

99 个回复

  • 非常实用的经验,值得学习和参考!书中提到的温度对电容的影响较大比较认同。

    一些因素会引起电解电容失效,如极低的温度,电容温升(焊接温度,环境温度,交流纹波),过高的电压,瞬时电压,甚高频或反偏压;其中温升是对电解电容工作寿命(Lop)影响最大的因素。

    这篇文章说到了许多电工们的心中啊。电解电容确实受温度影响比较大,尤其在密闭空间内,电解质 蒸发较快,曾经受过这方面教训了,再加之国内的电解电容质量真不敢恭维,但是电解电容的用量尤其是电源上还是很广泛的。

    此外建议在滤波电路中,电容的耐压值不要小于交流有效值的1.42倍。另外还要注意的一个问题是工作电压裕量,一般来说要在15%以上。让电容的额定电压具有较多的余裕,能降低内阻、降低漏电流、降低损失角、增加寿命。

    另:现在TI做deyisupport投入精力很大啊,各地研讨会和网上活动都推广。哈哈电工们的福音啊!

  •  比较实用的一段经验总结.值得学习这中方式估计PF值能在0.9以上.损耗大大减少,用MOS来控制来也让成本达到了最小化,减少MOS管的导通阻抗,降低肖特基的压降,减少热敏的阻值,使用软开减少开关损耗,降低工作频率减少磁芯损耗.在正激和桥式电源中,磁芯损耗着重考虑涡流损耗。在反激变压器和储能电感中,既要考虑涡流损耗又要考虑磁滞损耗,尤其是DCM方式工作的电源,磁滞损耗是第一位的。所以可以确定,做电源时第一点就是根据电源的工作频率选取相应的磁芯材料,铜线的直径也不是越大越好。这是我们往常使用的方法

    我们都一样....

  •  该章主要讲解了如何精准的测量电源纹波,主要讲解几个小技巧。1 示波器开启带宽限制2.去掉探针帽3将示波器引线缠绕铁氧体磁芯周围。这些细小的注意会让纹波测量更准确。在极端情况下,电流短时流经 15 nH 电感和 10 μF 旁路电容的一英寸导体时,该滤波器的截止频率为 400 kHz。这种情况下,就意味着高频噪声将会得到极大降多情况下,该滤波器的截止频率会在电源纹波频率以下,从而有可能大大降低纹波。经验丰富的工程师应该能够找到在其测试过程中如何运用这种方法的途径。

  •  

    电源是电子电路稳定运行的基础,做出一款好的电源是电路设计成功的第一步,TI在这方面做的工作可谓细致,以前是通过一些视频教程来学习的,但当遇到问题是又不方便查阅,这次,TI对这些知识点进行了归纳整理,并汇编成书,实在是我们这些技术人员的一大幸事,这样即方便查阅,也方便系统的学习.对以后的工作的帮助是很大的.

    书中从各方面对电路设计的难点和注意事项都进行了详细的讲解,特别是对电源性能参与的测试测量方面,感觉讲的比较具体,特别是正确的测试方法才能得到准确的数据从来找到问题,优化设计,

    而TI通过这样的活动把这些知识点推广开来,对技术人员从事电源开发设计工作提供了很好的学习途径,对TI的了解和产品的优异性能也有了质的提升.最后祝贺活动贺圆满成功,也愿TI产品能给消费者带来更好的生活享受.

  •  在很多电源的测试中都会存在这样的问题,而且还存在在没接示波器的时候,电源能正常工作,接了示波器反而不能工作的情况。1、通过取掉探针“帽”,并构成一个拾波器,可以消除由长接地引线形成的天线;2、将一小段线缠绕在探针接地连接点周围,并将该接地连接至电源,缩短暴露于电源附近高电磁辐射的端头长度,从而进一步减少拾波。这是2种很常用的测试方法。

  •  本经验结合图形详细的介绍了同步整流可提高效率,同时也能够极大地帮助瞬态负载调节