This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2576-adj 负载太大时电感嗡鸣,输出不正常

Other Parts Discussed in Thread: LM2576

你好!

我用LM2576做12V转6V的电源,参考数据手册,电感落于68uH,47uH左右,我选用了47uH(但不清楚其额定电流)。

6V出来后还有后续稳压芯片分别做6v转5V,6v转3.3V;另外板子上还有另外一路12V转-5V。所有电源做在一块板上,主要负载是另外一块板,上面有运放电路(+5,-5),AD(5V),和CPLD(3.3V)等。

情况是这样的:

1)一开始-5V转换还没有实现,导致运放电路没有正常工作。这个时候可能负载比较小(?),+5V和+3.3V输出正常,AD和CPLD能正常工作。

2)后来修复了-5V输出,这个时候不接负载的话,各路转换电源都正常。接入负载后,运放能工作了,+5V输出正常,但+3.3V输出失效,具体表现为:

             a.上电瞬间,+3.3V有输出,因为有指示灯亮几秒种后+3.3V输出降为0V左右,同时,LM2576端电感开始鸣叫;

             b.2576输出6V正常,6V转5V正常,唯独6V转3.3V没有输出。

分析下来可能原因:1)电感值或其额定电流不够;2)LM2576有问题。但为什么同一个输入源,+6V转+5V(使用UCC-381)工作,+6转+3.3V(使用AMS1117)就失效了呢?

请帮助分析诊断,谢谢!