This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps61221效率问题

我使用TPS61221数据手册中的典型连接电路测试,输入1.5V左右电压,使能EN为0时,输出端有0.98V电压,不为0V?

实际应用中,输出电流12mA(3.3V)左右,输入端电流40mA(1.47V)左右,计算效率:(12*3.3)/(40*1.47)=67%左右,而参考数据手册,在这种应用情况下效率应>=80%,不知道是什么原因?在整个测试过程中效率在60%~80%之间,效率比数据手册中给出的要低。