Other Parts Discussed in Thread: TPS40055
Rt=820K,Rkff=270K,1脚和3脚之间的电阻是330K。输出电压5V15A,12V输入5V输出满载效率94%。就是启动电压问题无法解决。请各位老大帮忙分析,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS40055
Rt=820K,Rkff=270K,1脚和3脚之间的电阻是330K。输出电压5V15A,12V输入5V输出满载效率94%。就是启动电压问题无法解决。请各位老大帮忙分析,谢谢!
Hi
按照datasheet:http://www.ti.com.cn/cn/lit/ds/symlink/tps40055.pdf 第七页的公式计算,Rkff=221.5kohm, 可以取220kohm.
同时注意layout, 在尽量靠近Vin脚处layout一个10uF陶瓷电容稳压,2个至少22uF的陶瓷电容layout靠近MOS输入端,以及输入的储能电容330uF*2, 这些都是为了在瞬态变化时尽量稳定输入电压,使其能在Vin=8V时工作(防止电压被拉低)
Hi
另外在datasheet:http://www.ti.com.cn/cn/lit/ds/symlink/tps40055.pdf第十页有提供欠压保护的迟滞设计,也可以用来解决设计较为低的输入电压。
非常感谢Johnsin Tao
我现在从BP10电压反馈到KFF,KFF脚不接到Vin,本以为可以取消输入电压对占空比的影响,实际上输入电压依然对占空比有影响,是不是即使IC的外部KFF不与Vin有关联,内部的电路依然使占空比与Vin有关联。
Hi
不太明确你的意思,但是就占空比而言D=Vin/Vout, 肯定是跟Vin相关联的。
不太明白为何,当KFF脚不接Vin,而是接BP10脚,但是占空比依然与Vin有关联。
现在关键的问题是,KFF通过电阻接到BP10后,如果调节相连的电阻使其启动电压为9V,输出5V的时候,输入电压9-40V,都不会对输入电压有影响,但是如果输出电压设定为13.8V,这个时候输入电压要到20V,才有稳定的13.8V电压。要想输入电压为16V,输出电压能稳定输出13.8V,那么必须得调节KFF与BP10之间的电阻,但是调节这个电阻了,启动电压就会被提高了。现在的目的是想不需要调节KFF与BP10之间的电阻值,实现启动电压9V,输入电压16V的时候,输出电压能有稳定的13.8V。
Hi
首先向你明确一下降压芯片的工作,降压芯片只能做降压变化即输入电压必须比较输出电压高,例如9~40V转5V, 并且通常占空比不会达到100%。
TPS40055也是降压转换器,因此当13.8V输出时, 输入电压至少需要大于13.8V, 而 假设TPS40055在500 kHz ≤ fSW ≤ 1 MHz时最大占空比在80%, 按照之前的公式D=Vo/Vin <80% , 当Vo=13.8V, 此时必须Vin>13.8/80%=17.25V,接近20V附近。