Other Parts Discussed in Thread: TPS63060, TPS63060EVM-619
比如我想用TPS6360,标称最高输入电压是12V,最大耐压是17V。不知道能不能用在最高输出12.6V的锂电池上?
因为锂电特性,所以电压肯定不会超过12.6V,工作一会电压也会降下去,不知道这个5%的超标使用能不能用在正式产品里?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS63060, TPS63060EVM-619
比如我想用TPS6360,标称最高输入电压是12V,最大耐压是17V。不知道能不能用在最高输出12.6V的锂电池上?
因为锂电特性,所以电压肯定不会超过12.6V,工作一会电压也会降下去,不知道这个5%的超标使用能不能用在正式产品里?
感谢两位回复,因为要升降压,4-12.6V输入,5V输出,只有这颗芯片比较适合。
想了想还是放个1N4007在前面,降压使用。虽然整体效率低了一些,不过对电源效率需求不高,还可以防电源接反。
另外再请教:如果供电电源线比较(大概1米),每40ms,其中20ms需要输入电流200mA,另外20ms需要输入电流700mA(输出电流略低,因为常规使用4-6V输入,5V输出,输入输出输出电流不会差太多)
除了规格书上推荐的20uf输入电容外,是否还需要加大容量的固态电解来平稳输入电压吗?大概需要多少容量?
输出电容推荐的是22uf×3,也需要再加吗?
对电源了解不多,还请指点,免得走了弯路,非常感谢!
Hi
输入2个10uF陶瓷电容够了,输出采用3个22uF电容也足够。
但是需要注意因为你的输入采用了较长的导线,可能存在较大的寄生电感,这样在TPS63060的输出可能存在非常大的震荡电压,甚至烧芯片,您需要确认。
所以你需要注意你导线的选择,同时在导线的输出处增加一个330uF甚至更大的电容来稳压。(可以在调试中注意一下)。
Hi
其次对于上述,因为采用12.6V供电,超过芯片推荐的12V供电,而采用二极管是可行的,尽管它影响效率。
但是我个人认为12.6V供电可以考虑不增加二极管,原因是Vin脚的最高耐压是17V,也就是17V之后才是高风险。datasheet推荐的测试电压Vdd采用的是12Vmax, 这个通常是有buffer的,个人认为超标5%,是低风险。如果不是很在意效率的情况下,增加二极管完全符合datasheet,当然是最安全的。
非常感谢!想与您再确认一下,是在【输出】加一个比如470uF的固态电解电容吗?我还以为是在输入端加电容,因为在TPS63060EVM-619这份demo板的电路图里看到,是在输入端加了一个100uF的电容。
因为推荐的电感不好找,我选了个Vishay的IHLP-2525CZ-01,http://www.vishay.com/docs/34104/lp25cz01.pdf,是不是只要电感能支持高频【Frequency range up to 5.0 MHz】,就没问题吧?
再次感谢。
Hi
在芯片的Vin脚layout 20uF的陶瓷电容就足够瞬态稳定可。 100uF电容其实只要是考虑到输入源到板子上这部分供电的影响,正如我之前提到如果你是采用导线供电,在导线的输出端增加一个330uF甚至更大的电容一样,可以滤除寄生电感所导致的震荡电压或者说是稳压。
电感如你所选,这样类似的功率电感都是可以的。