Other Parts Discussed in Thread: UCD3138PSFBEVM-027, UCD3138
您好:请问UCD3138PSFBEVM-027提供的原理图,更改一下器件参数后是否也适用大点功率(2KW 110V 20A)的DC/DC设计?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: UCD3138PSFBEVM-027, UCD3138
您好:请问UCD3138PSFBEVM-027提供的原理图,更改一下器件参数后是否也适用大点功率(2KW 110V 20A)的DC/DC设计?谢谢!
刚开始调试到这里,现在遇到这样两个问题:前面您说的将firmware修改部分可以用,具体怎么实现?
一、首先问题是如何获得UCD3138EVM-027的UCD3138里的固件firmware?用FUSION_DIGITAL_POWER_DESIGNER吗还是DEVIDE GUI?具体怎么操作?
二、目前看FUSION_DIGITAL_POWER_DESIGNER或者DEVIDE GUI都不识别新的EVM-030,是否应该先下载才能识别?
三、如果是的话,是不是可以先用FUSION_DIGITAL_POWER_DESIGNER选择PFSP模板建立工程文件,然后下载到EVM-030中?但工程文件是*..XML文件, 而DEVICE GUI下载需要.X0文件,不知道怎么操作??
四、能否给提供一份源代码,非常需要!
这个UCD3138真的感觉很复杂,又没有更多的渠道获得帮助,现在剩余的开发时间已经很紧张了,可到现在怎么用还没完全弄懂呢,真的很着急,麻烦尽早给予答复,谢谢了!