Other Parts Discussed in Thread: OPA847
您好:
我使用TPS7A4901和TPS7A3001为5个OPA847运放供电,正电压输入是+24v,输出是+5v,负电压输入-6v,输出是-5v,上电后发现,-5v输出正常,
+5v输出上下跳动严重,TPS7A4901发烫严重,将OPA847减少为2个,+5v输出正常,但依然发烫。但是OPA847得电流只要18mA,而TPS7A4901可以达到
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Max Han 说:假如你带4个运放,每个运放20mA,压差为24-5=19V,所以LDO的功耗为19*0.02*4=1.52W,这么大的损耗,如果散热还没做好,你说能不热吗?
不是电流能力不够,是���温,这与LDO的原理有关
建议先用DC/DC将24V降下来,再用LDO降至5V
Hi Max:
你好,非常感谢您的帮助,我已确认thermal pad焊接没问题,请问您的意思是,即使thermal pad焊接没问题,如果用24V的话,散热依然会很大,所以必须先将24V降下来才行,那一般将到多少合适?12V?,我看datasheet上说,7A4901输入可达到36V,除了降压还有没有其他的办法,板子已经做出来了,就这样废了,心疼啊!
Hi
按照上述的计算1.5w左右的功耗,如果采用Junction-to-ambient的热阻55℃/W, 那么芯片的问题=Ta+Pd*Rq=25+1.5*55=107℃.
还没有到达芯片的热保护问题,说明直接的负有载可能大于20mA, 或者实际的热阻是超过55℃/W, 除了PowerPad要充分与GND铜箔焊接好之外,这个GND还要尽量扩张面积(相当于扩大散热片面积),甚至要打孔连接背面的Gnd.
如上,降低输入电压是可以减小功耗的,例如你将输入电压减低到8~10V,功耗就是20mA*(10-5)*4=0.4W, 芯片的温度就是25+0.4*55=52℃
所以你可以在LDO前面增加一级DC/DC,尽量减低LDO的输入,甚至降低到5.5V(只要大于LDO的输出5V加上LDO的最大Vrop, 100mA时最大Vdrop小于500mV,当然您还可以再稍微留点裕度)
Hi
按照上述的计算1.5w左右的功耗,如果采用Junction-to-ambient的热阻55℃/W, 那么芯片的问题=Ta+Pd*Rq=25+1.5*55=107℃.
还没有到达芯片的热保护问题,说明直接的负有载可能大于20mA, 或者实际的热阻是超过55℃/W, 除了PowerPad要充分与GND铜箔焊接好之外,这个GND还要尽量扩张面积(相当于扩大散热片面积),甚至要打孔连接背面的Gnd.
如上,降低输入电压是可以减小功耗的,例如你将输入电压减低到8~10V,功耗就是20mA*(10-5)*4=0.4W, 芯片的温度就是25+0.4*55=52℃
所以你可以在LDO前面增加一级DC/DC,尽量减低LDO的输入,甚至降低到5.5V(只要大于LDO的输出5V加上LDO的最大Vrop, 100mA时最大Vdrop小于500mV,当然您还可以再稍微留点裕度)