This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运放供电使用LM2611产生的-5V电压

Other Parts Discussed in Thread: LM2611

我用LM2611产生 -5V电压给运放供电,原理图如下,但是实际输出,1.4MHz的纹波有12mV以上,请问可能是什么问题呢?布局?还是我两个电感和CCUK值选的不对呢?实际电路输出端我又加了几个小电容和穿心电容,不过纹波基本没变。这可能是什么问题呢?

L4和L5还有C52的值是怎么选定的呢?我看数据手册和应用手册里给出的值也不一样。

我打算用一个DCDC产生-9V到-6V的负压,然后用一个LDO升到-4V到-5V,这样做对纹波和噪声抑制有好处吗?有没有相关的DCDC和LDO推荐呢