TPS54340电路原理图如下
,默认条件下Vfb为0.8v。现在我欲在FB接的PRJ端子上强行注入恒流源以达到软件控制输出,经测试,电流注入成功,Vfb电压也增加,但是输出VOUT却降低了,不知为何?还望各位高人指点
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS54340电路原理图如下
,默认条件下Vfb为0.8v。现在我欲在FB接的PRJ端子上强行注入恒流源以达到软件控制输出,经测试,电流注入成功,Vfb电压也增加,但是输出VOUT却降低了,不知为何?还望各位高人指点
请问注入的电流是多少,Vfb电压又增加了多少?电流注入后,计算Vout时会多一项 ' - IR5 ',可能使Vout降低。
原来的Vout=Vfb*(R5+R6)/R6,注入电流后Vout=Vfb'*(R5+R6)/R6-IR5,其中I是你注入电流的大小。从公式看,如果IR5比dVfb*(R5+R6)/R6大的话,Vout是会降低的。
不注入电流和注入电流的电流流向是怎样的呢?还有Vfb的电压值会一直固定在0.8v吗?
Vfb基准是0.8V,如果Vfb升高,占空比会减少,来使输出保持不变,所以强制注入电流使Vfb升高的话,占空比应该会减少。
FB脚是误差放大器的负脚,因为是high impedence脚,所以电流可以当作是从Vout流向地。
如果你想改变输出电压的话,调节R5电阻会比较好。
可以先前调节R5是的输出电压较大,然后用程序PID算法来达到控制输出的目的。