我把之前通过dlp4500的GUI生成的bin文件下载到DLP4710EVM中,然后软件提示状态变成了“connected,power off”状态,按“sw21”的话d56会闪一下然后熄掉,我想问下这块怎么操作?然后我的bmp格式的图片如何使用DLP4710EVM的GUI生成它需要的固件,以及设置投射的patte?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我把之前通过dlp4500的GUI生成的bin文件下载到DLP4710EVM中,然后软件提示状态变成了“connected,power off”状态,按“sw21”的话d56会闪一下然后熄掉,我想问下这块怎么操作?然后我的bmp格式的图片如何使用DLP4710EVM的GUI生成它需要的固件,以及设置投射的patte?
您好!
感谢使用TI的DLP产品。
1.请从如下页面下载DLP4710-LC EVM最新的GUI软件和固件,在连接电源并且关闭电源开关的情况下Upload firmware.
http://www.ti.com.cn/tool/cn/dlp4710evm-lc#technicaldocuments
2.目前还没有发布DLP4710-LC GUI软件的说明手册,但是可以参考DLP3010-LC的Internal Control的说明。
http://www.ti.com.cn/cn/lit/ug/dlpu074/dlpu074.pdf
谢谢