Hi,
板卡:自制DLP4710,2片3479, 搭配 3005
状态:连接光机,排线和LED线均已检查连接准确,单片机已烧写程序,
问题:连接GUI软件状态显示正常,但是光机不工作,开机后不投影,切换Splash Image或者显示pattern,只闪烁微弱红光,
这边查到DLPA3005的 ILLUM_A路输出电压值为1.8V,不足以点亮DMD,请问该怎样调解ILLUM的输出电压值?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
板卡:自制DLP4710,2片3479, 搭配 3005
状态:连接光机,排线和LED线均已检查连接准确,单片机已烧写程序,
问题:连接GUI软件状态显示正常,但是光机不工作,开机后不投影,切换Splash Image或者显示pattern,只闪烁微弱红光,
这边查到DLPA3005的 ILLUM_A路输出电压值为1.8V,不足以点亮DMD,请问该怎样调解ILLUM的输出电压值?
您好!
感谢使用TI的DLP产品。
如果能够连接GUI软件并且发送I2C命令,说明系统启动完成,请问HOST_IRQ信号的状态是怎么样的(正常情况下会先拉高再拉低)。
1.首先请确认LED是否使能?在Display->IntelliBright页面下检查
2.检查系统电源轨是否正常,包括DLPC3479和DLP4710的电源是否正常
3.LED通常是电流驱动的,ILLUM_A的输出电压与LED的电流以及伏安特性等相关,不能直接调节电压
4.请问目前使用的固件是官网的固件吗?
5.如果检查LED已经使能且电源都正常,请问是否方便提供原理图,可以私信给我。
Best regards