Other Parts Discussed in Thread: DLPA2005, DLPC3470, DLP2010
使用DLP2010EVM-LC參考設計,量測spi讀flash讀一下就停止了,量DMD_LS_CLK也是跑一陣子就沒有了,Voffset、Vbias、Vreset電壓沒有出來,启动过程一直没完成,不知道可能的问题在哪里?希望TI工程师能指点一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
感谢使用TI的DLP产品。
如下点可以检查:
1.是否正确连接了DMD和LED。
2.检查Proj_on是否拉高,INTZ、RESETZ是否为高?
3.DLPA2005输出的1.1V/1.8V/3.3V等电压是否正确输出且稳定
4.固件是否正确,如果设计与参考设计类似,可以从如下链接下载
http://www.ti.com/tool/DLP2010EVM-LC
Best regards
您好!
3.很抱歉没有表达清楚,需要检测的是DLPC3470和DLP2010需要的所有电压是否正常(除了VBIAS/VOFFSET/VRST)。
4.EVM上同样是Option3,并且Option并不会造成启动问题。
另外,
请问目前测试过多少驱动板?多少光机(是否有使用光机厂商提供的固件测试过)?是否有能够开机的系统?
与参考设计相比做了哪些修改?如果方便的话也可以提供原理图,私信给我。
Best regards