你好,我们刚买了一个DLP LightCrafter 4500 作学习用途,想了解它可能用到的配件及型号,以便购买,请问能给我列个清单吗?谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我们刚买了一个DLP LightCrafter 4500 作学习用途,想了解它可能用到的配件及型号,以便购买,请问能给我列个清单吗?谢谢~
感谢购买DLP Lightcrafter4500 EVM。
EVM并不包含需要的电源、连接线缆和其他可选的硬件组件。要使用该EVM进行产品开发,下面是必要的配件:
1. 电源,规格如下
– Nominal voltage: 12-V DC
– Typical current: 6 A
– Maximum current: 7 A
– DC connector size:
• Inner diameter: 2.5 mm
• Outer diameter: 5.5 mm
• Shaft: 9.5-mm female, center positive
– Efficiency level: V
– Reommended power supply is Digi-Key part number 62-1186-ND , or equivalent.
2. USB线缆:A-miniB USB
可选组件:Pandaboard 4500 (https://www.svtronics.com/panda?product_id=43)
如需了解进一步的信息,请参考Lightcrafter4500用户手册。
如采用DLP技术做三维机器视觉系统开发,还需要搭配工业摄像头进行系统设计。相关的参考设计,请浏览http://www.ti.com/tool/tida-00254
希望能对你有所帮助。
您好!
投影镜头不推荐更换。
请参考
http://www.deyisupport.com/question_answer/dlp_mems/f/106/p/122881/411842.aspx#411842