Other Parts Discussed in Thread: TMS320DM648
硬件:TMS320DM648
软件:CCS5.4 NDK2.0.0
问题描述:在使用TCP/IP协议栈的时候,创建socket后,循环使用send函数持续发送数据。但是发送过一段时间后send函数返回错误并退出,错误类型为EWOULDBLOCK,请问这种错误是因为什么导致的(内存不够?),以及怎么解决?
1. Socket配置代码:
// Create the main TCP socket
stcp = socket(AF_INET, SOCK_STREAM, 0);
if( stcp == INVALID_SOCKET )
{
printf("Fail socket, %d\n", fdError());
goto leave;
}
// Set Pmort = 9528, IP address = IPAddrSend
IPAddr = inet_addr(RemoteIPAddr);
bzero( &sin1, sizeof(struct sockaddr_in) );
sin1.sin_family = AF_INET;
sin1.sin_len = sizeof( sin1 );
sin1.sin_addr.s_addr = IPAddr;
sin1.sin_port = htons(9528);
to.tv_sec = 5;
to.tv_usec = 0;
setsockopt( stcp, SOL_SOCKET, SO_SNDTIMEO, &to, sizeof( to ) );
setsockopt( stcp, SOL_SOCKET, SO_RCVTIMEO, &to, sizeof( to ) );
uart_write("connect to the server:");uart_write(RemoteIPAddr);
while(connect( stcp, (PSA) &sin1, sizeof(sin1) ) < 0)
{
printf("Fail connect, %d\n", fdError());
}
uart_write("Success!\n");
2. Send任务
while(1)
{
if( ((bytes = send( stcp, pBuf , (int)FRAME_SIZE, 0 )) < 0) )
{
printf("send failed (%d)\n",fdError());
goto leave;
}
if(FRAME_SIZE != bytes)
{
printf("send bytes (%d)\n",bytes);
}
totalBytes += bytes;
// Get TSK_idle time to compute CPU load half-way through
// number of packets transfers
if ( loop == count)
{
THRLOAD_getTskTime(&TSK_idle, &tskTime, &totalTime);
}
}
3. 发送任务出错执行的代码段: (send(...)函数内 --> SockSend(....)函数内)
// Check blocking condition
if( SizeCopy < size && !AddCopy )
{
// We need to block (protocol did not handle the data )
// Can't block a non-blocking socket
// If we timeout, we have an error and break the loop
if( (ps->StateFlags & SS_NBIO) || (flags & MSG_DONTWAIT) ||
!FdWaitEvent( ps, FD_EVENT_WRITE, ps->TxTimeout ) )
{
error = EWOULDBLOCK;
break;
}
}
就是在int SockSend( HANDLE h, char *pBuf, INT32 size, int flags, INT32 *pRetSize )函数中(在sock.c文件),这个函数我的理解是:先检查发送缓冲区是否有空间然后进行数据copy。如果没有空间就进入到上述3中的代码段阻塞等待……如果超时就报错退出,如果产生了可以写的事件则继续copy数据去发送。
注:在发送时出现上述错误退出后,使用的NDK库并没有关闭socket,并且客户端再也无法通过套接字连接DSP了