1、8168需要使用多个电源。在芯片内部,各电源之间是否有反偏二极管?
2、现在想用EN5367为8168供电,主要用于3.3V、1.0CON、1.5V。但是该DCDC不支持预偏置(pre-bias)功能,如果8168内部各电源之间有二极管的话,是否不能使用这种DCDC?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、8168需要使用多个电源。在芯片内部,各电源之间是否有反偏二极管?
2、现在想用EN5367为8168供电,主要用于3.3V、1.0CON、1.5V。但是该DCDC不支持预偏置(pre-bias)功能,如果8168内部各电源之间有二极管的话,是否不能使用这种DCDC?
谢谢!
你好,
DM8168的AVS的电源提供必需使用支持AVS的芯片。
其他的电源需要严格满足芯片的上电时序就可以。当然电压必须满足spec的要求。
Chris Meng 你好:
非常感谢。那就是不用考虑预偏置的问题了?
还有一个疑问:8168的各个电源都是从0V开始上电的吗?
延伸一下:如果DSP或者FPGA的电源不是从0V开始上电的话,此时是否必须使用带预偏置功能的芯片,才能为其供电?