1. 6678中共有3组DMA,分别是DMA0,DMA1,DMA2,每组有多少个通道数和队列数,以及SHADOW Regions和Global Region与这些DMA的关系是什么?
2.在使用DMA1时,使用不同的通道数但使用相同的队列(Event Queue)这样会发生冲突吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 6678中共有3组DMA,分别是DMA0,DMA1,DMA2,每组有多少个通道数和队列数,以及SHADOW Regions和Global Region与这些DMA的关系是什么?
2.在使用DMA1时,使用不同的通道数但使用相同的队列(Event Queue)这样会发生冲突吗?
1 每个CC对应的TC通道数如下:
EDMA3CC0 has two transfer controllers: EDMA3TC1 and EDMA3TC2.
EDMA3CC1 has four transfer controllers: EDMA3TC0, EDMA3TC1, EDMA3TC2, and EDMA3TC3.
EDMA3CC2 has four transfer controllers: EDMA3TC0, EDMA3TC1, EDMA3TC2, and EDMA3TC3
EDMA3CC将其地址空间划分为8个区域(Regions),从每个Region的地址空间都可以访问EDMA3CC的寄存器。即尽管物理上这些寄存器只有一份,但可以通过8个shadow region空间来访问。用户可以设置某个Region只能访问(R/W)这些Register的哪些bit,访问没有授权的bit是无效的。Region机制相当于提供了一个Filter给用户,通过每个shadow region去R/W这些CC的寄存器,只对授权的bit起作用。这样,尽管这些寄存器物理上只有一份,但不同的region去操作它们互不影响
2 会,TCn和event queue n 是一一对应的。