问题:
C6678LE的板子,上周五连还可以,今天下午连的时候,仿真器三个LED灯一起闪烁(D1D2D3,红绿黄),电脑无法检测到仿真器连接,无论是USB口看还是test connection尝试。网上一些帖子说是安全模式,尝试了之后报错。好着急,不会是我把板子玩坏了吧...
板子闪烁图:
连接无法检测:
在CCSV6中test connection的错误日志:
[Start: Blackhawk XDS560v2-USB Mezzanine Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\ZWJ\AppData\Local\TEXASI~1\CCS\
ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: emulator was not found
Download failed for file C:\ti\ccsv6\ccs_base\common\uscif\xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
[End: Blackhawk XDS560v2-USB Mezzanine Emulator_0]
尝试调整安全模式的错误: