This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助。C6678,CCS8.3编译问题,不知道缺少哪个库文件还是什么东西,求大神帮忙看一下

Description Resource Path Location Type
gmake: *** [core0_bios_0725_0508.out] Error 1 core0_bios_0725_0508    C/C++ Problem
gmake: Target 'all' not remade because of errors. core0_bios_0725_0508    C/C++ Problem
null: errors encountered during linking; "core0_bios_0725_0508.out" not built core0_bios_0725_0508    C/C++ Problem
null: unresolved symbols remain core0_bios_0725_0508    C/C++ Problem
program will not fit into available linker.cmd /core0_bios_0725_0508/Debug/configPkg line 214 C/C++ Problem
unresolved symbol EVM_init, first referenced in G:\wjm\code\core0_bios_0725_0508\Debug\configPkg\package\cfg\helloWorld_pe66.oe66 core0_bios_0725_0508    C/C++ Problem
unresolved symbol GPIO8_ISR, first referenced in G:\wjm\code\core0_bios_0725_0508\Debug\configPkg\package\cfg\helloWorld_pe66.oe66 core0_bios_0725_0508    C/C++ Problem
unresolved symbol main, first referenced in C:\ti\ti-cgt-c6000_8.3.2\lib\rts6600_elf.lib<args_main.c.obj> core0_bios_0725_0508    C/C++ Problem
unresolved symbol StackInit_Tsk, first referenced in G:\wjm\code\core0_bios_0725_0508\Debug\configPkg\package\cfg\helloWorld_pe66.oe66 core0_bios_0725_0508    C/C++ Problem
unresolved symbol Udp_send2_tsk, first referenced in G:\wjm\code\core0_bios_0725_0508\Debug\configPkg\package\cfg\helloWorld_pe66.oe66 core0_bios_0725_0508    C/C++ Problem

  • 具体是编译的什么工程?版本是什么?是否做过修改?

    这个库文件在该路径下能找到吗?是不是没有添加到工程中去。

    G:\wjm\code\core0_bios_0725_0508\Debug\configPkg\package\cfg\helloWorld_pe66.oe66

    program will not fit into available linker.cmd 

    是自己修改了CMD文件吗?

  • 你好,编译的是前工程师留下的工程,基于helloword工程修改的。我现在在搭建环境,编译出现问题。编译器版本是TI V8.3.2。XDCtools是3.32.2.25,bios6.46.5.55.CMD文件应该是修改过的。 .my_msmcsram2: load > MSMCSRAM3
    .gFrame: load > L2SRAM
    .shareDDR3RAM2: load > DDR3SDRAM2 align = 0x0
    .sharedDDR3RAM4: load > DDR3SDRAM4
    xdc.meta: load > MSMCSRAM3, type = COPY
    其中.sharedDDR3RAM4: load > DDR3SDRAM4前面有红色叉子提示有错误。但是现在我还没有弄明白是什么意思。是库里的设置和cmd有冲突吗
  • 跟库文件没有关系,内存分配可能有些问题,建议先看一下以下链接第七章节的memory部分。
    www.ti.com/.../spruex3u.pdf
  • 您好 我用helloworld这个例程 编译后出现Description Resource Path Location Type
    gmake.exe: *** [package/cfg/helloWorld_pe66.oe66] Error 2 helloworld_evmc6678l C/C++ Problem
    请问这种问题应该怎么处理?
    我在ccs中查看debug-configPkg-packages-cfg文件夹 发现没有helloWorld_pe66.oe66 于是手动添加了它到cfg文件夹中 但是一编译这个文件就消失 然后还是报这个错误