This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6487采用SGMII口与Marvel 88e1111相连,SGMII回环成功,但是就是发不出数据



现象描述:TCI6487采用SGMII口与Marvel 88e1111相连,SGMII回环成功,但是就是发不出数据。
问题描述:1)怀疑是物理层初始化的问题,88e1111的寄存器需要做什么配置?(我现在只配置寄存器0的值为0x8140,参照C6474EVM)
          2)88e1111硬件配置是否正确?(cfg0-6分别为001,100,111,011,100,000,参照c6678EVM)
   3)是否与SGMII的初始化有关?(SGMII的初始化参照c6474EVM)

  • 你检查一下MDIO口的状态?

  • 你好,我猜你有C6487的Demo板卡上的代码,然后想porting到C6474的demo板卡上。 C6487和C6474是几乎一样的芯片,但是两款Demo板卡在PHY芯片的连接上略有不同。我已经帮客户做过类似的porting工作。

    下面供你免费参考:

    /////////////////////////////////////////////////////////////////////////////////

    SgmiiCfg.txConfig = 0x00000e23;
    /*SERDES specific config (0x00081021) */
    /* NO autoneg. */

    SgmiiCfg.modeOfOperation = SGMII_MODE_OF_OPERATION_WITHOUT_AN;

    if (SGMII_config(&SgmiiCfg) != 0) {

    ..............

    }

    /* Configure PHY port 6 SERDES --> Faraday 1 at 1000mpbs, full duplex */
    MDIO_phyRegWrite(0x0e, 0, 0x8140);
    /* Force internal switch --> port 6 SERDES to 1000MBPS, full Duplex */
    MDIO_phyRegWrite(0x16, 0x1, 0x043e);
    /* Force 1000mps at copper PHY, disable auto-negotiate*/
    MDIO_phyRegWrite(0x01, 0, 0x8140);

    ///////////////////////////////////////////////////////////////////////////////////////////////////////////////

    Br

    william.dong@enea.com

  • 非常感谢你的回复!

    我现在是想把spectrum digital inc的C6474EVM的代码移植到自己开发的TCI6487上,由于采样phy芯片为88e1111,与c6474EVM采样的88e6122有很大的不同,是不是只要修改phy_init()里的代码就行了? 

     

    void phy_init()
    {
        /* ---------------------------------------------------------------- *
         *                                                                  *
         *  Init PHY / MDIO                                                 *
         *                                                                  *
         * ---------------------------------------------------------------- */
        MDIO_CONTROL = 0x4000001f;              // Enable MII interface

        // Turn PPU off to make copper PHY visible at SMI address 0x01
     phy_setReg(27, 4, 0x0081);

     // Configure Marvell 88E6122 PHY
        phy_setReg(0xe, 26, 0x47);    // Set PHY port 6 SERDES to 0.7V swing
        phy_setReg(0xd, 26, 0x47);    // Set PHY port 5 SERDES to 0.7V swing
     phy_setReg(0x0e, 0, 0x8140);  // Configure PHY port 6 SERDES --> Faraday 1 at 1000mpbs, full duplex
     phy_setReg(0x0d, 0, 0x8140);  // Configure PHY port 5 SERDES --> Faraday 2 at 1000mbps, full duplex
        phy_setReg(0x15, 0x1, 0x043e);  // Force internal switch --> port 5 SERDES to 1000MPBS, full Duplex
        phy_setReg(0x16, 0x1, 0x043e);  // Force internal switch --> port 6 SERDES to 1000MBPS, full Duplex

     // Force 1000mps at copper PHY, disable auto-negotiate
    // phy_setReg(1, 0, 0x8140); // 0x8140 = 1000mbps

     // Force 100mps at copper PHY, disable auto-negotiate
     phy_setReg(1, 0, 0xa100); // 0xa100 = 100mbps

        // Wait for link establishment
        phy_wait( 4000000 );
    }

    C6474EVM上两片分别接5port和6port,上面设置的物理地址怎么这么多,不是应该只有两个?88e1111的物理地址是通过外部引脚配的,是固定的,如何去写这部分的代码?

    非常期盼你的回复