This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于dm365 UBL中修改运行频率的问题



我修改了dm365的ubl,让芯片降频运行在ARM216_DDR173_OSC19P2 频率下,程序运行到启动内核时停止:

## Booting kernel from Legacy Image at 80700000 ...
   Image Name:   Linux-2.6.32.17-davinci1-g2b4942
   Created:      2014-01-15   1:32:11 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2201516 Bytes = 2.1 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux............................................................................................................................................... done, booting the kernel.

请问在ubl中修改频率后内核需要做什么修改