This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168管脚USB0_R1的设置问题?



在评估板中,此管脚命名为USB0_TXRTUNE,硬件指导手册对此管脚的描述如下:USB0 current reference output. When the USB0
peripheral is used, this pin must be connected via a 44.2-Ω ±1% resistor to VSS.When the USB0 PHY is powered down, this pin
should be left unconnected.但评估板原理图中是用10K电阻下拉到底,请问该管脚该如何设置?