nand write.e 和nand write.yaffs有什么区别啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我昨天晚上用write.e烧写yaffs2文件系统映像到开发板中,出现了下面的错误:
DM6467 EVM > boot
NAND read: device 0 offset 0x500000, size 0x220000
2228224 bytes read: OK
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.32-rc2-davinci1-g73dbf
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2039444 Bytes = 1.9 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux.............................................................
....................................................................... done, bo
oting the kernel.
Linux version 2.6.32-rc2-davinci1-g73dbf71-dirty (root@bbs) (gcc version 4.2.0 (
MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #14 PREEMPT Wed Jun 11 09:40:09 CS
T 2014
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DM646x EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci dm6467_rev3.x variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512
Kernel command line: noinitrd root=/dev/mtdblock3 rw rootfstype=yaffs2 init=/li
nuxrc console=ttyS0,115200
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 128MB = 128MB total
Memory: 125496KB available (3808K code, 329K data, 136K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 249.03 BogoMIPS (lpj=1245184)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 43 gpio irqs
NET: Registered protocol family 16
MUX: Setting register STSOMUX_DISABLE
PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
MUX: Setting register STSIMUX_DISABLE
PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
MUX: Setting register PTSOMUX_DISABLE
PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
MUX: Setting register PTSIMUX_DISABLE
PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
MUX: initialized CIR_UART2
MUX: Setting register CIR_UART2
PINMUX1 (0x00000004) = 0x00000000 -> 0x00000020
MUX: initialized UART0_GPIO_36_37_38_8
MUX: Setting register UART0_GPIO_36_37_38_8
PINMUX1 (0x00000004) = 0x00000020 -> 0x00000021
MUX: initialized UART1_GPIO_25_26
MUX: Setting register UART1_GPIO_25_26
PINMUX1 (0x00000004) = 0x00000021 -> 0x00000025
MUX: initialized UART2_GPIO_39_40_41_42
MUX: Setting register UART2_GPIO_39_40_41_42
PINMUX1 (0x00000004) = 0x00000025 -> 0x00000035
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
vpif vpif: vpif probe success
Switching to clocksource timer0_1
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc: USB Host mode controller at fec64000 using DMA, IRQ 13
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
yaffs Jun 4 2014 09:57:36 Installing.
Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
msgmni has been set to 245
io scheduler noop registered
io scheduler anticipatory registered (default)
DMA: DMA_devInit()
DMA:install success, major num = 252
CIR device registered successfully (Major = 251, Minor =
0)
[XKL_GPIO_DRIVER]:dm6467_gpio initialized
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c20000 (irq = 40) is a ST16654
console [ttyS0] enabled
serial8250.0: ttyS1 at MMIO 0x1c20400 (irq = 41) is a ST16650V2
serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ4
2): -22
brd: module loaded
loop: module loaded
at24 1-0050: 32768 byte 24c256 EEPROM (writable)
NAND device: Manufacturer ID: 0xec, Chip ID: 0x76 (Samsung NAND 64MiB 3,3V 8-bit
)
Scanning device for bad blocks
Bad eraseblock 252 at 0x0000003f0000
Bad eraseblock 256 at 0x000000400000
Bad eraseblock 260 at 0x000000410000
Creating 4 MTD partitions on "davinci_nand.0":
0x000000000000-0x000000020000 : "params"
mtd: Giving out device 0 to params
0x000000020000-0x000000160000 : "bootloader"
mtd: Giving out device 1 to bootloader
0x000000500000-0x000000900000 : "kernel"
mtd: Giving out device 2 to kernel
0x000000900000-0x000004000000 : "filesystem"
mtd: Giving out device 3 to filesystem
davinci_nand davinci_nand.0: controller rev. 2.2
spi_davinci spi_davinci.0: DaVinci SPI driver in EDMA mode
Using RX channel = 17 , TX channel = 16 and event queue = 3
at25 spi0.0: 32 KByte at25640a eeprom, pagesize 64
spi_davinci spi_davinci.0: Controller at 0xfec66800
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
dm9000 Ethernet Driver, V1.31
console [netcon0] enabled
netconsole: network logging started
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbtest
mice: PS/2 mouse device common for all mice
rtc-pcf8563 1-0051: chip found, driver version 0.4.3
rtc-pcf8563 1-0051: rtc core: registered rtc-pcf8563 as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
cs4954 1-0000: chip found @ 0x0 (DaVinci I2C adapter)
tvp5158 1-005e: [tvp5158 probe]: chip found @ 0xbc (DaVinci I2C adapter)
tvp5158_checkChip ok!
Patch is downloading...
Patch is downloaded. Soft reset!
using default mode PAL!
tvp5158_initVideoMode successfully!
tvp5158_initAudioMode devId=0 successfully!
vpif_capture vpif_capture: registered sub device tvp5158-0
tvp5158 1-005f: [tvp5158 probe]: chip found @ 0xbe (DaVinci I2C adapter)
tvp5158_checkChip ok!
Patch is downloading...
Patch is downloaded. Soft reset!
using default mode PAL!
tvp5158_initVideoMode successfully!
tvp5158_initAudioMode devId=1 successfully!
vpif_capture vpif_capture: registered sub device tvp5158-1
vpif_capture vpif_capture: DM646x VPIF Capture driver initialized
watchdog watchdog: heartbeat 60 sec
Advanced Linux Sound Architecture Driver Version 1.0.21.
[coolen_debug](cs4341_i2c_probe).
[coolen_debug](cs4341_register).
[coolen_debug](davinci_mcasp_probe): txnumevt = 0.rxnumevt=0
[coolen_debug](davinci_mcasp_probe): playbackCH = 6.
[coolen_debug](davinci_mcasp_probe): captureCH = 9.
[coolen_debug](davinci_mcasp_probe): txnumevt = 0.rxnumevt=0
[coolen_debug](davinci_mcasp_probe): playbackCH = 12.
[coolen_debug](davinci_mcasp_probe): captureCH = -1.
[coolen_debug](cs4341_probe).
[coolen_debug](cs4341_init):gpioRet = 0.gpio value 2
[coolen_debug](cs4341_init): cs4341 regList:
CS4341_REG_MODE:0
CS4341_REG_MCLKDIV:0
CS4341_REG_TMIX:8c
CS4341_REG_AVOLUME:0
CS4341_REG_BVOLUME:0
asoc: cs4341 <-> davinci-i2s mapping ok
[coolen_debug](evm_cs4341_init).
ALSA device list:
#0: DaVinci DM6467 EVM (cs4341)
TCP cubic registered
NET: Registered protocol family 17
Clocks: disable unused emac
Clocks: disable unused timer1
davinci_emac_probe: using random MAC addr: 1a:77:de:0c:50:9c
emac-mii: probed
rtc-pcf8563 1-0051: low voltage detected, date/time is not reliable.
rtc-pcf8563 1-0051: retrieved date/time is not valid.
rtc-pcf8563 1-0051: hctosys: invalid date/time
yaffs: dev is 32505859 name is "mtdblock3"
yaffs: passed flags ""
yaffs: Attempting MTD mount on 31.3, "mtdblock3"
yaffs: auto selecting yaffs1
yaffs_read_super: isCheckpointed 0
VFS: Mounted root (yaffs2 filesystem) on device 31:3.
Freeing init memory: 136K
Warning: unable to open an initial console.
Failed to execute /linuxrc. Attempting defaults...
Kernel panic - not syncing: No init found. Try passing init= option to kernel.
Backtrace:
[<c002e6d0>] (dump_backtrace+0x0/0x110) from [<c002e814>] (dump_stack+0x18/0x1c)
r6:00000000 r5:c002560c r4:c0409450
[<c002e7fc>] (dump_stack+0x0/0x1c) from [<c0040164>] (panic+0x54/0x124)
[<c0040110>] (panic+0x0/0x124) from [<c002a578>] (init_post+0xd4/0xfc)
r3:c6103f00 r2:c03e4520 r1:000000c0 r0:c038390c
[<c002a4a4>] (init_post+0x0/0xfc) from [<c00087cc>] (kernel_init+0xe0/0x110)
r4:c0408d00
[<c00086ec>] (kernel_init+0x0/0x110) from [<c0043240>] (do_exit+0x0/0x654)
r5:00000000 r4:00000000
请问一下,这是因为烧写命令的原因,还是根文件系统本身的原因啊?
一般可能是这两种情况:
1.需要使用nand write.yaffs命令烧写
2.mkyaffs2image工具或者制作时的参数为问题
可以先增加u-boot对nand write.yaffs的支持,这个网上的资料很多,如果还有错误,再检查工具。
http://processors.wiki.ti.com/index.php/Put_YAFFS_Image_to_Flash
http://processors.wiki.ti.com/index.php/Create_a_YAFFS_Target_Image