This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于OTG



我们的开发版上画了一个MINI B的母口USB,原理图如下:

 当内核配置这个口为主模式的时候,通过OTG线接U盘可以识别(OTG一端是MINI B plug,另外一端是Standard A类型的母口)

但是配置成从模式的时候,没有任何反应。从模式时候的内核的关键配置是:

  <M> Sbull Device Support

--- USB support

<*>   Inventra Highspeed Dual Role Controller (TI, ADI, ...)

 <*>     TI81XX                                                  
            TI81XX usb connector's ID pin control (from software settin
            Driver Mode (USB Peripheral (gadget stack))  --->

<*>   USB Gadget Support  --->

--- USB Gadget Support

 (2)   Maximum VBUS Power usage (2-500 mA)

       USB Peripheral Controller (Inventra HDRC USB Peripheral (TI)

<M>   USB Gadget Drivers

 <M>     File-backed Storage Gadget

 [*]       File-backed Storage Gadget testing version

然后系统启动过程加载g_file_storge.ko,加载命令如下:

mkdosfs -v /dev/sbulla 2>/dev/null
mkdir /mnt/ramdisk 2>/dev/null
mount -t vfat /dev/sbulla /mnt/ramdisk 2>/dev/null
insmod g_file_storage.ko file=/dev/sbulla stall=0 removable=1

执行这些命令之后的输出是:

g_file_storage gadget: No serial-number string provided!
g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010
g_file_storage gadget: Number of LUNs=1
g_file_storage gadget-lun0: ro=0, nofua=0, file: /dev/sbulla

使用一端是MINI B plug,另外一端是Standard A plug的usb线连接到笔记本(linux系统和winXP系统都测试过),没有任何反应。

在linux系统下执行lsusb没有任何多出的信息,在winXP的设备管理器下,插拔没有出现任何新设备。

使用万用表测试USB1_VBUS旁边的电阻R475是有接近5v的电压,而USB1_DRV_VBUS是0