Other Parts Discussed in Thread: TVP5158
你好:
我想问一下,我怎样测试我的TVP5158是否正常工作,在TI的代码里是否有相应的测试程序。我是从摄像头输入在VGA上显示。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TVP5158
你好:
我想问一下,我怎样测试我的TVP5158是否正常工作,在TI的代码里是否有相应的测试程序。我是从摄像头输入在VGA上显示。谢谢!
是针对 在TI的代码里是否有相应的测试程序 这个问的啊。
不知道你是什么主平台啊,怎么帮你找有没有测试程序。。。
你好:
不好意思,我是DM8168的板子,用的是EZSDK的代码。谢谢!
如果你不用DM8168实际采集的结果来测试的话,那么可以通过
1. 通过I2C访问TVP5158内部的状态寄存器来判断5158的工作情况
2. 测量5158的VP输出来推断是否正常输出。
Table 4-2. Status 1
Table 4-3. Status 2
Table 4-10. Video Standard Status 看是否和输入匹配
你好:
因为EZSDK里没有支持TVP5158的驱动,我参考7002和DVR里的5158写了一个驱动。我的目的是为了测试我写的这个驱动是否可以适合5158.所以想要一个测试程序。
我是想用DM8168实际采集的结果来测试,是否有其他的方法。至于你上面讲的向寄存器里写值我已经可以写了。谢谢!
您好,我现在做的也是基于sdk的5158的驱动,能留下您的qq号或联系方式方便联系吗