大家好;
请问aac 的adts数据流中adts_buffer_fullness应当如何来理解;应当如何来进行计算呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
请参考:ISO/IEC 14496-3 以及 ISO/IEC 13818-7标准中的描述,希望对你有所帮助。
adts_buffer_fullness : state of the bit reservoir in the course of encoding the ADTS frame, up to and including the first raw_data_block() and the optionally following adts_raw_data_block_error_check(). It is transmitted as the number of available bits in the bit reservoir divided by NCC divided by 32 and truncated to an integer value (Table 9). A value of hexadecimal 7FF signals that the bitstream is a variable rate bitstream. In this case, buffer fullness is not applicable.
AAC编码器源码下面一段是关于ADTS头信息的:
A value of hexadecimal 7FF signals that the bitstream is a variable rate bitstream (VBR)。
/* Variable ADTS header */
PutBit(bitStream, 0, 1); /* copyr. id. bit */
PutBit(bitStream, 0, 1); /* copyr. id. start */
PutBit(bitStream, hEncoder->usedBytes, 13);
PutBit(bitStream, 0x7FF, 11); /* buffer fullness (0x7FF for VBR) */
PutBit(bitStream, 0, 2); /* raw data blocks (0+1=1) */
http://www.audiocoding.com/downloads.html