This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

./system_server &运行是错误



大家好!我用的是dm365 EVM开发板,IPNC V5.1,在运行./system_server &时出现了如下错误信息:

queue id:196608                                                                 
FileMngThread created                                                           
Creat queue id:229377                                                           
queue id:229377                                                                 
AlramThread created                                                             
Share memory init success                                                       
IPNC_DM365EVM_5.1.0 (root@123456) (gcc version 4.3.3 (GCC) ) #6 PREEMPT Wed Ju  
Creat queue id:262146                                                           
queue id:262146                                                                 
queue id:229377                                                                 
queue id:262146                                                                 
Creat queue id:294915                                                           
queue id:294915                                                                 
net_search_gateway:eth0, 1A8C0, 0, 1                                            
net_search_gateway:eth0, 0, FE01A8C0, 3                                         
                                                                                
CPU is DM365                                                                    
                                                                                
*****************************************************************               
                                                                                
  IPNC BUILD VERSION: DM365 IPNC RDK V5.10.00.04                                
                                                                                
*****************************************************************               
                                                                                
Check_device_version : DEVICE VER = 1 !!                                        
Error: SemWait: Invalid Semaphore handler                                       
Error: SemRelease: Invalid Semaphore handler                                    
./av_server.out DM365 NTSC TI2A AEWB 720P H264 4000000 VBR AUTO MENUOFF &       
ApproDrvInit: 7                                                                 
queue id:131076                                                                 
                                                                                
 DM365MM Init Successful                                                        
AVSERVER UI: Initializing.                                                      
                                                                                
 CLK Hz,                                                                        
 ARM   Hz =  216000000                                                          
 DDR   Hz =  172500000                                                          
 VPSS  Hz =  172500000                                                          
 IMCOP Hz =  172500000                                                          
                                                                                
 [OSA_FILE ] Reading file [/mnt/nand/IMG_Paramset.bin] ... ERROR                
IMAGE TUNE: Paramset File is not available..... Setting DEFAULT parameter       
 ERROR  (imageTuneCommunication.c|IMAGE_TUNE_ServerOpen|119): IMAGE TUNE 2      
 ERROR  (drv_imageTune.c|DRV_imageTuneInit|91): IMAGE_TUNE_ServerOpen()         
 ERROR  (drv.c|DRV_init|70): IMAGE TUNE init                                    
 ERROR  (drv.c|DRV_init|102): DRV_init()                                        
 ERROR  (avServerApi.c|AVSERVER_init|630): DRV_init()                           
 ERROR  (avServerUi.c|UI_start|85): AVSERVER_init() 

希望大家帮帮忙,将感激不尽!

  • 你好,

    请问你在EVM上有接sensor么?如果没有,你是否有修改Rules.make来使能SYSTEM_PLATFORM := EVM么?EVM上支持的是TVP514x,你的log显示的是720p的配置。你打印的错误是Image tuning tool初始化的时候报错了。

  • 你好!我的EVM上接了sensor,在Rules.make中也使能了SYSTEM_PLATFORM := EVM,下面是我Rales.make的配置:

    # Select Hardware Platform: EVM or IPNC
    SYSTEM_PLATFORM := EVM
    #SYSTEM_PLATFORM := IPNC

    # IPNC Platform Device needs to selected
    IPNC_DEVICE := DM365
    #IPNC_DEVICE := DM368
    #IPNC_DEVICE := DM369
    #IPNC_DEVICE := DMVA1
    #IPNC_DEVICE := DMVA2

    # Filesystem mode to selected: NAND or NFS
    FILESYS_MODE := NFS
    #FILESYS_MODE := UBIFS

    # Build configuration : debug or release
    #APP_BUILD_CFG    := debug
    APP_BUILD_CFG   := release

    # UBIFS mtd-utils mode
    MTD_UTILS_MODE := 64bit
    #MTD_UTILS_MODE := 32bit

    # Sensor Selected for the build, based on SYSTEM_PLATFORM
    # IPNC and EVM platform have different set of Sensor supported
    ifeq ($(SYSTEM_PLATFORM), IPNC)
    IMGS_ID := IMGS_MICRON_MT9P031_5MP
    #IMGS_ID := IMGS_MICRON_MT9D131_2MP
    #IMGS_ID := IMGS_OV10630_1MP
    #IMGS_ID := IMGS_MICRON_MT9M031_1.2MP
    #IMGS_ID := IMGS_MICRON_MT9M034_1.2MP
    #IMGS_ID := IMGS_OV2715_2MP
    #IMGS_ID := IMGS_SONY_IMX035_1_3MP
    #IMGS_ID := IMGS_SONY_IMX036_3MP
    #IMGS_ID := IMGS_SONY_IMX104_1_3MP
    #IMGS_ID := IMGS_SONY_IMX136_2_3MP
    #IMGS_ID := IMGS_SONY_IMX122_2_3MP
    #IMGS_ID := IMGS_AR0130_1.2MP
    #IMGS_ID := IMGS_AR0330_3.1MP
    #IMGS_ID := IMGS_AR0331_3.1MP
    #IMGS_ID := IMGS_AR0331_3.1MP_WDR
    #IMGS_ID := IMGS_PANASONIC_MN34041_2.1MP
    endif
    ifeq ($(SYSTEM_PLATFORM), EVM)
    IMGS_ID := IMGS_TVP514X
    #IMGS_ID := IMGS_MICRON_MT9P031_5MP
    endif

    # This flag will determine whether any 2A modules is required in build or not
    #AEWB_BUILD_MODE := no
    AEWB_BUILD_MODE := yes

    # WiFi hardware mode flag: ON or OFF
    # ON:if WiFi Hardware module is present else this needs to be set to OFF
    #WIFI_MODULE_MODE := ON
    WIFI_MODULE_MODE := OFF

    # AES Encyrption mode flag: ON or OFF
    # ON:if AES Encyprtion module is present else this needs to be set to OFF
    #AES_MODULE_MODE := ON
    AES_MODULE_MODE := OFF

    # Face Recognition flag: ON or OFF
    # ON:if Face Recognitio module is present else this needs to be set to OFF
    #FACE_RECOG_MODE := ON
    FACE_RECOG_MODE := OFF

    # Sensor Board Vendor: Appro or Leopard Imaging
    # APPRO:if Appro Sensor Board is used or LIMG: if Leopard Imaging Board are used
    SENSOR_BOARD_VENDOR := APPRO
    #SENSOR_BOARD_VENDOR := LIMG

    # Build warnings will be treated as errors for av_capture folder
    TREAT_WARNINGS_AS_ERROR := no
    #TREAT_WARNINGS_AS_ERROR := yes

    而[OSA_FILE ] Reading file [/mnt/nand/IMG_Paramset.bin] ... ERROR                
    IMAGE TUNE: Paramset File is not available..... Setting DEFAULT parameter这个错误,

    我的根文件系统下面没有/mnt/nand/IMG_Paramset.bin这个文件,能否告诉我TVP514X它支持的分辨率是多少,还有那个720P应该在哪修改,谢谢!!



  • 你好,

    老版本的IPNC软件是在EVM上验证过的,但最新的就不一定了。TVP514x输入分辨率只有D1,而且是隔行的。

    IPNC的软件最好还是在IPNC参考设计上测试运行。

    或者你可以找找IPNC v2.6的代码在EVM上试试看。

  • Chris Meng 你好,我参考了这篇帖子https://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/t/337634修改了参数为./av_server.out DM365 NTSC TI2A AEWB 736 576 H264 4000000 VBR AUTO MENUOFF &结果还是一样

  • 上述问题已经解决,原因是./av_server.out 参数设置错误,具体请参考Collaterals文件夹下YUV_Sensor_Integration_Guide_IPNC_DM36x文档,但是为什么会出现

    这样的错误:

    ./av_server.out DM365 DEI  AEWB D1 H264 3000000 VBR AUTO MEN
    UOFF

     DM365MM Init Successful
    AVSERVER UI: Initializing.
     
     CLK Hz,
     ARM   Hz =  216000000
     DDR   Hz =  172500000
     VPSS  Hz =  172500000
     IMCOP Hz =  172500000
     
     [OSA_FILE ] Reading file [/mnt/nand/IMG_Paramset.bin] ... ERROR
    IMAGE TUNE: Paramset File is not available..... Setting DEFAULT parameter

     DM365MM Init SuccessfulSYSTEM.MSTPRI0 value changed to 00440011

    CONFIGURING AVSERVER FOR DM365 .....
    queue id:32769
    Floating point exception


    文档中说EVM只支持NFS模式,指的是文件系统需要NFS挂载?我是同过内核烧写进flash的,NFS挂载没有成功,有没有遇到这种问题的

  • 查看源码可知 D1后面的参数指定宽度和高度,正确的参数应为./av_server.out DM365 DEI APPRO2A AEWB D1 736 576 H264 3000000 VBR AUTO MENUOFF