This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何增大dm36X的内存



TI的大神你们好:

        在uboot中设置启动参数setenv bootargs 'mem=48M  ,会指定内存大小,但是我的DDR显示的内存为DRAM:  128 MB,我想修改指定内存48M,发现不传参数或改变48M的值都无法启动系统,

提示:

DM365 IPNC :>setenv bootargs 'mem=64M console=ttyS1,115200n8 noinitrd ip=192.168.1.168:192.168.1.46:192.168.1.1:255.255.255.0:::off rw ubi.mtd=3,2048 rootfstype=ubifs root=ubi0:rootfs cmemk.phys_start=0x83000000 cmemk.phys_end=0x88000000 cmemk.phys_start_1=0x00001000 cmemk.phys_end_1=0x00008000 cmemk.pools_1=1x28672 cmemk.allowOverlap=1 cmemk.useHeapIfPoolUnavailable=1 nohz=off highres=off clocksource=acpi_pm lpj=1077248 eth=20:8D:6F:00:00:10 quiet'
DM365 IPNC :>saveenv
Saving Environment to NAND...
Erasing Nand...
Erasing at 0x300000 -- 100% complete.
Writing to Nand... done
DM365 IPNC :>boot

Loading from NAND 128MiB 3,3V 8-bit, offset 0x500000
Image Name: Linux-2.6.37_IPNC_DM365_5.1.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3448160 Bytes = 3.3 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.37_IPNC_DM365_5.1.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3448160 Bytes = 3.3 MB
Load Address: 80008000
Entry Point: 80008000
Loading Kernel Image ... OK
OK

Starting kernel ...

[ 0.347779] DRV: Module install successful
[ 0.347815] DRV: Module built on Aug 4 2015 15:46:18
[ 0.354359] CMEMK Error: Failed to request_mem_region(0x83000000, 83886080)
[ 0.836289] Error: Driver 'davinci-mcbsp' is already registered, aborting...
INIT: version 2.86 booting

 坐等回复,谢谢

  • 你好,

    在DM36x的代码里面,除了保留给Linux的内存外,其他的内存都留给了cmem,cmem是为了提供连续的物理空间的utility。你可以修改insmod cmemk.ko后面的参数来减少划给cmem的内存。但有可能在运行代码时候出现cmem空间不够的错误。

  • 谢谢你的回复,我试试

  •   请问一下 sd卡录像时,1分钟打一次包,会随机出现Error: Memory return Invalid,导致录像进程Appro_avi_save退出。这个会不会是由于cmem引起的

  • 默认的DM36X代码是没有使用cmemk.ko吗?,我没有在我们的文件系统中找到,我在IPNC5.1代码中以下文件中找到该驱动,默认传给cmem的内存是多少,我要加载驱动使用下面那个,参数的单位是字节吗?

    ./dvsdk_ipnctools/codecs-dm365/packages/ti/sdo/codecs/mpeg2enc/apps/client/build/arm926/cmemk.ko

    ./dvsdk_ipnctools/codecs-dm365/packages/ti/sdo/codecs/mpeg4enc_hdvicp/apps/client/build/arm926/cmemk.ko
    ./dvsdk_ipnctools/codecs-dm365/packages/ti/sdo/codecs/mpeg4dec_hdvicp/apps/client/build/arm926/cmemk.ko
    ./dvsdk_ipnctools/codecs-dm365/packages/ti/sdo/codecs/mpeg2dec/apps/client/build/arm926/cmemk.ko
    ./dvsdk_ipnctools/codecs-dm365/packages/ti/sdo/codecs/h264dec/apps/client/build/arm926/cmemk.ko
    ./dvsdk_ipnctools/codecs-dm365/packages/ti/sdo/codecs/vc1dec/apps/client/build/arm926/cmemk.ko
    ./dvsdk_ipnctools/codecs-dm365/packages/ti/sdo/codecs/h264enc/apps/client/build/arm926/cmemk.ko


  • 你好,

    2.6.18的kernel使用的cmem module.

    2.6.37 kernel把cmem编译到kernel里面了。配置是在uboot里面做的。例如下面黄色部分:

    setenv bootargs 'mem=48M console=ttyS1,115200n8 noinitrd ip=dhcp rw ubi.mtd=3,2048 rootfstype=ubifs root=ubi0:rootfs cmemk.phys_start=0x83000000 cmemk.phys_end=0x88000000 cmemk.phys_start_1=0x00001000 cmemk.phys_end_1=0x00008000 cmemk.pools_1=1x28672 cmemk.allowOverlap=1 cmemk.useHeapIfPoolUnavailable=1 nohz=off highres=off clocksource=acpi_pm lpj=1077248 eth=00:0C:0C:A0:07:DF'

  • 你好,

    这个uboot命令代表分给cmem总内存80M,然后后面的是什么意思,是不是内存都充分利用了

    我在我的板子中用top查看内存和cpu发现一下奇怪的现象,内存使用率有超过100%的,能告诉我是为什么吗?谢谢


    506 1 root S 210m 474% 25% ./av_server.out DM365 NTSC BOARDVER=2 
    815 468 root S 28448 63% 8% ./Appro_avi_save /mnt/mmc/ipnc/2015-08
    532 504 root S 26428 58% 1% ./wis-streamer -s -h 
    530 504 root S 26428 58% 1% ./wis-streamer -s -h 
    529 504 root S 26428 58% 1% ./wis-streamer -s -h 
    504 1 root S 26428 58% 1% ./wis-streamer -s -h 
    468 1 root S 98200 217% 1% ./system_server 
    812 692 root R 3080 7% 1% top 
    660 1 root S 1764 4% 0% avahi-autoipd: [eth0] bound 169.254.2.
    579 2 root SW 0 0% 0% [mmcqd/0]
    531 504 root S 26428 58% 0% ./wis-streamer -s -h 
    4 2 root SW 0 0% 0% [kworker/0:0]
    655 1 root S 44468 98% 0% ./boa -c /etc 
    692 1 root S 3080 7% 0% -sh 
    508 1 root S 2976 7% 0% /usr/sbin/inetd 
    687 1 root S 2964 7% 0% /sbin/syslogd -n -C64 -m 20 
    690 1 root S 2900 6% 0% /sbin/klogd -n 
    681 1 root S 2900 6% 0% /usr/sbin/telnetd 
    664 1 root S 2704 6% 0% avahi-daemon: running [192.local] 
    668 1 root S 2276 5% 0% ./upnp-scanip

  • james ZHANG1 说:

    这个uboot命令代表分给cmem总内存80M,然后后面的是什么意思,是不是内存都充分利用了

    Linux使用48M,加上cmem用的80M,正好是128MB。

    后面使用的地址是DM36x ARM的internal memory。

  •        谢谢你的回复,你的回复对我帮助很大,不知道你有没有弄过wifi移植,有的话麻烦帮我回答一下这个问题.

    http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/92229.aspx

    谢谢