问题1:
http://software-dl.ti.com/processor-industrial-sw/esd/PRU-ICSS-PROFIBUS-SLAVE/latest/index_FDS.html
PRU-ICSS Profibus Slave Windows Installer
该网址下载下来的解压后通过配置脚本生成的profibus_slave Project 能否实现profibus slave这样的功能?DPV1能否可以达到?
按照说明文档里面该APP仅能完成 通过提供的UART接口配置从地址的功能.
问题2:
将生成的Project 导入到CCS9.1中编译生成.out文件如何烧录到AMIC110上?烧录选项是否有特殊要求?是否需要烧录到特定核心?
比如Pru0/1or A8上. 如果是,那么如何修改烧录的相关配置选项?
若该回复解决了您的问题,请点击“确认此为答案”,谢谢。
回复 Shine:
回复 Damon_Gu:
那对应的bootloader 工程是否有,我使用的是C:\ti\pdk_am335x_1_0_16\packages\ti\starterware\bootloader 路径下的程序源码,但是编译不通过,您这边可否提供下相对应的AMIC110的bootloader spi 启动的CCS工程文件 谢谢!!!
回复 yongqing wang:
#error Unsupported boot mode !!gmake: *** [sbl_copy.o] Error 1gmake: *** [sbl_mcspi.o] Error 1gmake: Target 'all' not remade because of errors.recipe for target 'sbl_copy.o' failedrecipe for target 'sbl_mcspi.o' failedrequest for member 'image_size' in something not a structure or unionrequest for member 'load_addr' in something not a structure or unionrequest for member 'load_addr' in something not a structure or unionunknown type name 'ti_header'