This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x更换nand后启动不了



最近按照客户需求扩大nand容量,之前自己做的AM335X板子使用镁光的4g容量MT29F4G08ABADA,这次更换为8g容量MT29F8G08ABACA。

4g容量的pagesize为2048b,obb大小64b,8g容量的pagesize为4096b,obb大小224b,请问修改uboot中nand配置需要注意些什么,我修改完使用sd卡烧写uboot

后断电重启,串口打CC,写操作每次都显示OK,但事实上没写成功,不知道什么原因

  • 你的写操作是什么?怎么知道它没写成功?

    在文件中 Am335x_evm.h (include\configs) 修改相关参数:

    #ifdef CONFIG_NAND
    /* NAND: device related configs */
    #define CONFIG_SYS_NAND_5_ADDR_CYCLE
    #define CONFIG_SYS_NAND_PAGE_COUNT (CONFIG_SYS_NAND_BLOCK_SIZE / \
    CONFIG_SYS_NAND_PAGE_SIZE)
    #define CONFIG_SYS_NAND_PAGE_SIZE 2048
    #define CONFIG_SYS_NAND_OOBSIZE 64
    #define CONFIG_SYS_NAND_BLOCK_SIZE (128*1024)

  • 感谢您的回复!  我使用SD卡启动到uboot下,使用nand write 写MLO,再使用nand read 读

    U-Boot# nand write 0x81000000 0x0 0x20000

    NAND write: device 0 offset 0x0, size 0x20000
    131072 bytes written: OK

    U-Boot# nand read 0x81000000 0x0 0x20000

    NAND read: device 0 offset 0x0, size 0x20000

    ...

    ECC: uncorrectable.
    ECC: uncorrectable.
    NAND read from offset 0 failed -74
    0 bytes read: ERROR

    您说的地方也都改了,看起来是ECC错误,那么ECC部分如何修改

    #define CONFIG_SYS_NAND_PAGE_SIZE 4*1024 //2048
    #define CONFIG_SYS_NAND_OOBSIZE 224 //64
    #define CONFIG_SYS_NAND_BLOCK_SIZE (256*1024)//(128*1024)
    #define CONFIG_SYS_NAND_BAD_BLOCK_POS NAND_LARGE_BADBLOCK_POS
    #define CONFIG_SYS_NAND_ECCPOS { 2, 3, 4, 5, 6, 7, 8, 9, \
    10, 11, 12, 13, 14, 15, 16, 17, \
    18, 19, 20, 21, 22, 23, 24, 25, \
    26, 27, 28, 29, 30, 31, 32, 33, \
    34, 35, 36, 37, 38, 39, 40, 41, \
    42, 43, 44, 45, 46, 47, 48, 49, \
    50, 51, 52, 53, 54, 55, 56, 57, }

    #define CONFIG_SYS_NAND_ECCSIZE 512
    #define CONFIG_SYS_NAND_ECCBYTES 14

    8g容量的nand手册上看到

    Minimum required ECC 8-bit ECC per 540 bytes of data

    标红的部分应该怎么改

  • 配置如下:

    #define CONFIG_NAND_OMAP_ECCSCHEME  OMAP_ECC_BCH16_CODE_HW
    #define CONFIG_SYS_NAND_ECCBYTES 26
    #define CONFIG_SPL_NAND_AM33XX_BCH
    #define CONFIG_SYS_NAND_ECCSIZE 512
    #define CONFIG_SYS_NAND_ECCPOS	\ {
      2, 3, 4, 5, 6, 7, 8, 9, \
     10, 11, 12, 13, 14, 15, 16, 17, 18, 19, \
     20, 21, 22, 23, 24, 25, 26, 27, 28, 29, \
     30, 31, 32, 33, 34, 35, 36, 37, 38, 39, \
     40, 41, 42, 43, 44, 45, 46, 47, 48, 49, \
     50, 51, 52, 53, 54, 55, 56, 57, 58, 59, \
     60, 61, 62, 63, 64, 65, 66, 67, 68, 69, \
     70, 71, 72, 73, 74, 75, 76, 77, 78, 79, \
     80, 81, 82, 83, 84, 85, 86, 87, 88, 89, \
     90, 91, 92, 93, 94, 95, 96, 97, 98, 99, \
    100, 101, 102, 103, 104, 105, 106, 107, 108, 109, \
    110, 111, 112, 113, 114, 115, 116, 117, 118, 119, \
    120, 121, 122, 123, 124, 125, 126, 127, 128, 129, \
    130, 131, 132, 133, 134, 135, 136, 137, 138, 139, \
    140, 141, 142, 143, 144, 145, 146, 147, 148, 149, \
    150, 151, 152, 153, 154, 155, 156, 157, 158, 159, \
    160, 161, 162, 163, 164, 165, 166, 167, 168, 169, \
    170, 171, 172, 173, 174, 175, 176, 177, 178, 179, \
    180, 181, 182, 183, 184, 185, 186, 187, 188, 189, \
    190, 191, 192, 193, 194, 195, 196, 197, 198, 199, \
    200, 201, 202, 203, 204, 205, 206, 207, 208, 209, }
    
    
     在DT Bindings 配置

     ti,nand-ecc-opts="bch16" 
     ti,elm-id="<&elm> 

    在KConfigs 配置
    CONFIG_MTD_NAND_OMAP_BCH=y

  • 我的UBOOT使用的是psp6.0中的u-boot-2013.01.01-psp06.00.00.00,没有使用设备树配置,对于我使用的uboot版本,如何添加BCH16的支持

  •  先修改下面这些,uboot能正常驱动uboot了吗?

    #define CONFIG_NAND_OMAP_ECCSCHEME  OMAP_ECC_BCH16_CODE_HW
    #define CONFIG_SYS_NAND_ECCBYTES 26
    #define CONFIG_SPL_NAND_AM33XX_BCH
    #define CONFIG_SYS_NAND_ECCSIZE 512
    #define CONFIG_SYS_NAND_ECCPOS	\ {
      2, 3, 4, 5, 6, 7, 8, 9, \
     10, 11, 12, 13, 14, 15, 16, 17, 18, 19, \
     20, 21, 22, 23, 24, 25, 26, 27, 28, 29, \
     30, 31, 32, 33, 34, 35, 36, 37, 38, 39, \
     40, 41, 42, 43, 44, 45, 46, 47, 48, 49, \
     50, 51, 52, 53, 54, 55, 56, 57, 58, 59, \
     60, 61, 62, 63, 64, 65, 66, 67, 68, 69, \
     70, 71, 72, 73, 74, 75, 76, 77, 78, 79, \
     80, 81, 82, 83, 84, 85, 86, 87, 88, 89, \
     90, 91, 92, 93, 94, 95, 96, 97, 98, 99, \
    100, 101, 102, 103, 104, 105, 106, 107, 108, 109, \
    110, 111, 112, 113, 114, 115, 116, 117, 118, 119, \
    120, 121, 122, 123, 124, 125, 126, 127, 128, 129, \
    130, 131, 132, 133, 134, 135, 136, 137, 138, 139, \
    140, 141, 142, 143, 144, 145, 146, 147, 148, 149, \
    150, 151, 152, 153, 154, 155, 156, 157, 158, 159, \
    160, 161, 162, 163, 164, 165, 166, 167, 168, 169, \
    170, 171, 172, 173, 174, 175, 176, 177, 178, 179, \
    180, 181, 182, 183, 184, 185, 186, 187, 188, 189, \
    190, 191, 192, 193, 194, 195, 196, 197, 198, 199, \
    200, 201, 202, 203, 204, 205, 206, 207, 208, 209, }
  • 
    

    U-Boot 2013.01.01 (May 05 2017 - 11:00:08)

    I2C: ready
    DRAM: 512 MiB
    WARNING: Caches not enabled
    NAND: nand option: 0xd
    maf_id:0x2c
    dev_id:0xd3
    ret:0 busw: 0
    byte2:0x90
    byte3:0xa6
    byte4:0x64
    byte5:0x0
    byte6:0x0
    byte7:0x0
    else busw:0
    NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
    NAND 1GiB 3,3V 8-bit, sector size 256 KiB
    Page size 4096 b
    OOB size 224 b
    Erase size 262144 b
    nand scan : ret 0
    1024 MiB
    MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1

    按照您给的配置修改完,uboot卡在这了,而且看了下
    #define CONFIG_NAND_OMAP_ECCSCHEME  OMAP_ECC_BCH16_CODE_HW
    这个定义uboot中没有用到
  • 是这个CONFIG_NAND_OMAP_ECCSCHEME  没定义
    还是这个CONFIG_NAND_OMAP_ECCSCHEME 没定义 ?
  •  CONFIG_NAND_OMAP_ECCSCHEME
    是这个,整个uboot中没有用到这个定义
  • check了一下,发现你用的这个版本的uboot和kernel都不支持BCH16,较新的PDK是可以支持的

    To select ECC algorithm for NAND:

    U-Boot# nandecc [sw | hw <hw_type>]
    

    Usage:

    sw - Set software ECC for NAND hw <hw_type> - Set hardware ECC for NAND <hw_type> - 0 for Hamming code 1 for bch4 2 for bch8 3 for bch16 Currently we support only Software, Hamming Code and BCH8. We do not support BCH4 and BCH16 

    ECC schemes usage table

    ECC schemes usage table
    ComponentDefault ECC scheme used by the componentECC scheme to be used to flash the componentECC schemes supported by the component
    SPL BCH8 BCH8 BCH8
    U-boot Hamming BCH8 Hamming/BCH8
    Linux BCH8 BCH8 BCH8
    File System NA BCH8 NA
    Environment variables NA Hamming NA

  • 现在有点疑惑,am335x的ROM CODE是否支持镁光的MT29F8G08ABACA

    1 page = (4K + 224 bytes)
    1 block = (4K + 224) bytes x 64 pages = (256K + 14K) bytes
    1 plane = (256K + 14K) bytes x 2048 blocks= 4320Mb
    1 LUN = 4320Mb x 2 planes= 8640Mb
    manufacturer ID: 0x2c
    device ID      : 0xd3

  • 我可以帮你check 一下ROM code是否可以

    下面是这块NAND的指标参数对吧

  • 嗯,是的,那个oob  224b 很诡异,不知道uboot下如何配置

  • 可以尝试用新的PDK来驱动看看行不行,如果可以驱动成功,把MLO Uboot 写进去,看看能不能从Nand启动,也顺便证明了ROM core能不能驱动它

  • 我在am335x technical reference manul 手册26章中发现有这一句,Support for large page size (2048 bytes + 64 spare bytes) or very large page size 4096 bytes + 128 /218 spare bytes), 能否作为不支持该nand的依据

  • 这个NAND flash是可以支持的。

    首先为你解释一下什么是OOB。OOB Area (spare region) 的作用是为了实现ECC的功能,所保留在nand flash 每一page的空间大小: 

           当往某一款NAND Flash的page中写入数据的时候,假设这款NAND flash是每写256字节时候,我们生成一个ECC校验和,称之为原ECC校验和,需要保存到PAGE的OOB(out-of-band)数据区中。
      当从NAND Flash中读取数据的时候,每256字节我们生成一个ECC校验和,称之为新ECC校验和。
      校验的时候,根据上述ECC生成原理不难推断:将从OOB区中读出的原ECC校验和新ECC校验和按位异或,若结果为0,则表示不存在错(或是出现了ECC无法检测的错误);若3个字节异或结果中存在11个比特位为1,表示存在一个比特错误,且可纠正;若3个字节异或结果中只存在1个比特位为1,表示OOB区出错;其他情况均表示出现了无法纠正的错误。

  • 再跟你解析一下为什么AM335x可以支持这个nand flash:

    The MT29F8G08ABACA NAND 要求最小 8-bit ECC per 540 bytes of data. 我们ROM core可以满足这个要求,因为采用算法-- BCH8 algorithm, 是采用 14 bytes of ECC for every 512 bytes of data (112 bytes per 4k page)

    对于 4k 的page中,你的nand flash的OOB 是 224 bytes.

    OOB除了存ECC,还存有:.

    • Bad block marker for a bad block (mandatory),一般是2-bytes

    所以NAND flash 的OOB空间要求是…

    OOB Area (spare region) >= B * ( Page_Size / 512 ) + 2 

    where

    B =  8 bytes for BCH4

    B = 14 bytes for BCH8 ***

    B = 26 bytes for BCH16

    当我们用 BCH8 (8-bit ECC), 我们依然有 110 bytes 剩余

    当我们用BCH16 ,我们有14 bytes 剩余

    所以是可以使用这款Nand flash的

  • 谢谢您的指导,我仔细看了AM335x的技术手册,是支持的,我这边出错是很大原因是因为uboot中oob区相关的配置错误,像这些配置有没有什么资料可以参考参考

  • 这个链接可以参考一下,建议还是换成新的PDK,旧 的版本,4096page 的BH8好像不支持,我目前看到是这样的

    http://processors.wiki.ti.com/index.php/Linux_Core_NAND_User's_Guide

  • 楼主,你们用这款Nand Flash跑起来了吗?我们计划升级系统,Nand Flash也是选的这款。

    刚好我们的u-boot也是这个版本,我刚刚对了下代码,除了你修改的那些配置项,有一个地方要试一下:

    // u-boot/drivers/mtd/nand/nand_base.c
    
    /*
     * Get the flash and manufacturer id and lookup if the type is supported
     */
    static const struct nand_flash_dev *nand_get_flash_type(struct mtd_info *mtd,
    						  struct nand_chip *chip,
    						  int busw,
    						  int *maf_id, int *dev_id,
    						  const struct nand_flash_dev *type)
    {
    		.............................................
    		} else {
    			/* Calc pagesize */
    			mtd->writesize = 1024 << (extid & 0x03);
    			extid >>= 2;
    			/* Calc oobsize */
    			//mtd->oobsize = (8 << (extid & 0x01)) *
    			//	(mtd->writesize >> 9);
    			mtd->oobsize = 224;
    			extid >>= 2;
    			/* Calc blocksize. Blocksize is multiples of 64KiB */
    			mtd->erasesize = (64 * 1024) << (extid & 0x03);
    			extid >>= 2;
    			/* Get buswidth information */
    			busw = (extid & 0x01) ? NAND_BUSWIDTH_16 : 0;
    		}
    		.............................................
    }

    注意那个mtd->oobsize,按默认的算法计算出来的是128,但实际是224,所以,可以强制设置成224试一下。至于计算结果为什么会等于128,请参考附件Nand flash的datasheet,page 36 - 37:Table 10: READ ID Parameters for Address 00h --> Byte 3。

    另外,如果你的Nand flash已经写入了之前配置错误的MLO和u-boot,再次写之前一定要完全擦除,否则oob区可能已经被写坏了,新的MLO和u-boot同样无法启动。

    尝试完后,无论结果如何,还请回下贴。刚好我过两天就开始调试,大家多点交流。

    m71m_8gb_nand.pdf
  • Eggsy Pang,

    如果将8bits的MT29F8G08ABACA改成16bits的MT29F8G16ABACA可不可以呢!

    这么考虑的原因是,16bits的pagesize是2k,是不是就可以使用BCH8了?

    如果可以用BCH8,那么,换成16bits的后还有什么问题需要考虑,会不会由于其它原因,平台又不支持?

    以下是两个型号的基本参数:

    --------------------------------------------------------------------------------------------------------------------------------------------------------

    --------------------------------------------------------------------------------------------------------------------------------------------------------

  • Jesdy Hou 首先谢谢你的分享。

    我想下你用什么版本的SDK?

    关于第一个问题修改这个mtd->oobsize和不修改这个,你运行的结果有什么区别吗?

    第二个问题是硬件平台是可以支持的,只不过BCH8/16的在新的SDK支持性软件更好

  • Eggsy,

    我们的平台是TI-Android-ICS-4.0.3_AM335x_3.0.1,配套的u-boot是v2011.09版本,只支持1bit的Hamming码ECC校验。去年更换过一次Nand Flash,需要支持BCH8,所以移植了TI_Android_JB_4.2.2_DevKit_4.1.1中的u-boot,版本是v2013.01.01。Kernel到不用改,Android 4.0.3中带的Kernel就支持BCH8。

    关于mtd->oobsize,我还没测试,我们现在只是在做一些前期准备,Nand Flash样片申请中,估计这两天能拿到。

    不过昨天我发完贴后继续研究,发现除了楼主列出的那些参数,还有其它参数要修改,比如:

    1. eccsteps

    // u-boot/include/configs/am335x_evm.h
    
    #define CONFIG_SYS_NAND_ECCSIZE     512
    #define CONFIG_SYS_NAND_ECCBYTES    14
    
    //#define CONFIG_SYS_NAND_ECCSTEPS    4
    #define CONFIG_SYS_NAND_ECCSTEPS    8

    由于BCH8中eccsize是512,之前pagesize是2048,eccsteps为4,现在,pagesize是4096,eccsteps应该改成8。

    2. ecc_layout

    // u-boot/arch/arm/include/asm/arch-am33xx/omap_gpmc.h
    
    #define GPMC_NAND_HW_BCH8_ECC_LAYOUT {\
    	.eccbytes = 56,\
    	.eccpos = {2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15,\
    				16, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27,\
    				28, 29, 30, 31, 32, 33, 34, 35, 36, 37, 38, 39,\
    				40, 41, 42, 43, 44, 45, 46, 47, 48, 49, 50, 51,\
    				52, 53, 54, 55, 56, 57},\
    	.oobfree = {\
    		{.offset = 58,\
    		 .length = 6 } } \
    }
    
    // 改成
    
    #define GPMC_NAND_HW_BCH8_ECC_LAYOUT {\
    	.eccbytes = 112,\
    	.eccpos = {2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15,\
    				16, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27,\
    				28, 29, 30, 31, 32, 33, 34, 35, 36, 37, 38, 39,\
    				40, 41, 42, 43, 44, 45, 46, 47, 48, 49, 50, 51,\
    				52, 53, 54, 55, 56, 57, 58, 59, 60, 61, 62, 63,\
    				64, 65, 66, 67, 68, 69, 70, 71, 72, 73, 74, 75,\
    				76, 77, 78, 79, 80, 81, 82, 83, 84, 85, 86, 87,\
    				88, 89, 90, 91, 92, 93, 94, 95, 96, 97, 98, 99,\
    				100, 101, 102, 103, 104, 105, 106, 107, 108, 109,\
    				110, 111, 112, 113},\
    	.oobfree = {\
    		{.offset = 114,\
    		 .length = 110 } } \
    }

    这里应该有

    eccbytes = CONFIG_SYS_NAND_ECCBYTES * CONFIG_SYS_NAND_ECCSTEPS = 14 * 8 = 112,

    offset = eccbytes + 2 = 112 + 2 = 114,

    eccpos,从2依次填充,共112个,所以填充到113,

    length = CONFIG_SYS_NAND_OOBSIZE - offset = 224 - 114 = 110。


    如果以上修改过程会导致BCH8无法处理,那么,是不是意味着BCH8支持不了4k pagesize。


    暂时只发现以上这些,继续研究中......


    当然,kernel中相应的参数也应该同步修改。

  • Eggsy,

    另外,我们用的SDK也不支持device tree,要参照较新的SDK来移植BCH16也比较麻烦,所以,还是希望能使用BCH8,不知道TI有没有BCH8 patches去支持pagesize为4k的Nand flash?还请帮忙咨询下,谢谢!

  • 下面这个也要改下,MLO中要用到:

    // u-boot/include/configs/am335x_evm.h
    
    #define CONFIG_SYS_NAND_ECCPOS		{ 2, 3, 4, 5, 6, 7, 8, 9, \
    				10, 11, 12, 13, 14, 15, 16, 17, \
    				18, 19, 20, 21, 22, 23, 24, 25, \
    				26, 27, 28, 29, 30, 31, 32, 33, \
    				34, 35, 36, 37, 38, 39, 40, 41, \
    				42, 43, 44, 45, 46, 47, 48, 49, \
    				50, 51, 52, 53, 54, 55, 56, 57, }
    
    // 改成
    
    #define CONFIG_SYS_NAND_ECCPOS		{ \
    				2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, \
    				16, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27, \
    				28, 29, 30, 31, 32, 33, 34, 35, 36, 37, 38, 39, \
    				40, 41, 42, 43, 44, 45, 46, 47, 48, 49, 50, 51, \
    				52, 53, 54, 55, 56, 57, 58, 59, 60, 61, 62, 63, \
    				64, 65, 66, 67, 68, 69, 70, 71, 72, 73, 74, 75, \
    				76, 77, 78, 79, 80, 81, 82, 83, 84, 85, 86, 87, \
    				88, 89, 90, 91, 92, 93, 94, 95, 96, 97, 98, 99, \
    				100, 101, 102, 103, 104, 105, 106, 107, 108, 109, \
    				110, 111, 112, 113, }
  • 看起来make sense,可以尝试一下,如果不行,我这边帮你问下

  • 我觉得你可以这样测试:

    1.先把4096的nand flash 在Uboot阶段用BCH16来驱动,我想在新的或老的uboot版本都能够支持,应该是可以驱动起来。

    2.如果第一步骤成功了,再做用4096的nand 在uboot 阶段像你所说的那样修改,用BCH8启动,看一下效果。

    3.如果第一步骤成功, 第二步骤失败了,证明4096 nand一定要用BCH16来实现。

    4. 得到第三步骤的结论,你只能用2048的8g flash来搞了。

  • 好建议,我会做一下验证。

    如果验证结果表明BCH8不支持4k pagesize的话,只能改回2k pagesize的。

    那么,对于8Gb的 Nand flash来说,有两个选择:

    1. 一个就是前面我说的16 bits总线宽度的Nand flash,按你的说法,系统是支持的,是吧!我也看到代码里是有处理的。

    2. 另一个是使用两个die的Nand flash(如下图),总线宽度仍然为8 bits,不过代码里没有看到针对性的处理,不知道能不能支持。

  • 这个地方强制oob为224也配过了,还是不能从nand启动

  • 我这项目比较着急,没仔细去研究,不过在uboot中我也做过类似楼上的修改,始终都没有效果,不过我大部分时间是修改AM335X_starterware里的nand_flash_writer_AM335x.out源码,使用CCS调试的,不过也没出结果,你也可以试试,这样可以更直观一些。后来换了个8G2k页大小的nand,不需要修改任何地方,可以直接nand启动。

  • 请问你换的是哪个型号?

  • S34ML08G101TFI00,如果你有时间,可以研究一下镁光的,硬件工程师建议是使用镁光的,项目周期的原因选的这款

  • 早期我们是用三星和东芝1 bit ecc的,后来都停产了,就换成8 bits ecc的美光了,同时作了些对比,美光的基本没坏块,三星和东芝的一般3到10多个坏块。另外,在做开关机测试(20万次)时,三星和东芝平均5000~8000次文件系统就会损坏,而美光的20万次就出现过一次,显然,美光的稳定性确实很好。如果你们是用在工业场合的话,也建议你们使用美光的。

  • 我了解下S34ML08G101TFI00的参数,看看美光有没有比较一致的。你可以上传一下它的datasheet吗?

  • 刚刚查看了S34ML08G101TFI00的datasheet,它是1 bit ecc的,当然可以直接用。

    with 1 bit / 512 + 16 byte ECC


    这个8G其实是两个4G的die组成的。

  • 1. 一个就是前面我说的16 bits总线宽度的Nand flash,按你的说法,系统是支持的,是吧!我也看到代码里是有处理的。

    是 的,没错, 4096 page的用BCH16是支持的!

    2. 另一个是使用两个die的Nand flash(如下图),总线宽度仍然为8 bits,不过代码里没有看到针对性的处理,不知道能不能支持。

    这个2048page ,应该可以,请问它的device ID是多少

    看一下TAM手册是否支持,Table 26-14. Supported NAND Devices

  • nand ID 是D3,是支持的

  • 刚刚收到样片,不过代理商发错货,收到的不是MT29F8G08ABACA(Device ID:0xD3),而是MT29F8G08ABABA(Device ID:0x38),这个型号不在MPU的支持列表中,只能暂时做调试用。强制修改nand_flash_ids,添加对Device ID为0x38的支持,使用BCH8,按照前面我所说的修改,下载到Nand Flash后,MLO和u-boot运行均正常,Kernel启动到加载UBIFS时出现一连串的ECC错误:

    UBI error: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB 7:0, read 64 bytes

    UBI error: ubi_io_read: error -74 (ECC error) while reading 4096 bytes from PEB 7:4096, read 4096 bytes

    ...............................................................

    看来内核还需要进一步调试。

  • 再次感谢分享

    是可以支持的,因为这款NAND支持ONFI,所以即使不在那table里,ROM CORE也能读取。

    内核修改等待你测试的分享。

  • 总算拿到MT29F8G08ABACAWP(Device ID:0xD3)的样片了,换了两片试跑一下,系统可以正常启动,未出现任何错误。Kernel代码也不需要修改什么,还跟以前一样使用默认的BCH8即可。理论上,对于不支持ONFI的Nand Flash,需要将oobsize直接改成224,因为源码中那个算法算出的结果不对。

    -

    另外,前面一直忘了说了,由于Page size和Block size与之前用的2 Gbits的不一样:

    8 Gbits 2 Gbits
    Page size 4096 Bytes 2048 Bytes
    Block size 256 KBytes 128 KBytes

    所以,以下三点要修改:

    1. 对Flash重新分区,每个分区的起始地址和结束地址都必须“块对齐”,u-boot(包括环境变量)和kernel中修改必须一致;

    2. 所有与Page size和Block size相关的配置项;

    3. 制作UBIFS时的相关参数。

    每个点涉及的代码都不多,但有点散,这里就不贴出来了。

    -

    至于前面拿到的那个错误的样片 MT29F8G08ABABA(Device ID:0x38),Kernel启动时会出现ECC错误,简单调试了下没解决,就没管它了。

    主要不同是它的Block size是512 KBytes,还有就是Device ID不在MPU的支持列表中。

  • Jesdy

    请问 am335x_boneblack.dts 如何加入nand 支持 

    可以帮我看看我的问题吗,谢谢。 http://www.deyisupport.com/question_answer/dsp_arm/sitara_arm/f/25/t/137271.aspx


    James

  • 楼主,后面这个问题您解决了吗

  • Dear Hou工:

         我同样也在同一个芯片上遇到同一个问题,但是我尝试使用您的方法去修改,但是修改完了发现的 nandflash 烧入后坏块变的很多。

         不知道您还有没有相关的笔记,有偿咨询这个问题。