你好:
我新做了一块板子用的是3358的片子,采用的DDR2和NAND FLASH ,现在用CCS进行DEBUG时报错
(Error -1204 @ 0x3D5B)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 5.1.232.0)
我进行Test Connection 测试显示
显示没问题。
我板子 PWRONRESTn 和RTC_PWRONRESTn由FPGA提供,RTC_PWRONRESTn画图时没注意由FPGA的3V3的IO输出与要求不符合,要求为1V8,请问怎么排除问题。