无法安装filterpro软件



如图所示,好像是提示关于.notwork的相关错误

是版本对不上吗

请求协助

以下是install.log的内容

The following properties have been set:

Property: [AdminUser] = true {boolean}

Property: [ProcessorArchitecture] = Intel {string}

Property: [VersionNT] = 5.1.3 {version}

Running checks for package 'Windows Installer 3.1', phase BuildList

The following properties have been set for package 'Windows Installer 3.1':

Running checks for command 'WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe'

Result of running operator 'VersionGreaterThanOrEqualTo' on property 'VersionMsi' and value '3.1': true

Result of checks for command 'WindowsInstaller3_1\WindowsInstaller-KB893803-v2-x86.exe' is 'Bypass'

'Windows Installer 3.1' RunCheck result: No Install Needed

Running checks for package '.NET Framework 3.5 SP1', phase BuildList

Reading value 'SP' of registry key 'HKLM\Software\Microsoft\NET Framework Setup\NDP\v3.5'

Read integer value 0

Setting value '0 {int}' for property 'DotNet35SP'

The following properties have been set for package '.NET Framework 3.5 SP1':

Property: [DotNet35SP] = 0 {int}

Running checks for command 'DotNetFX35SP1\dotNetFx35setup.exe'

Result of running operator 'ValueGreaterThanEqualTo' on property 'DotNet35SP' and value '1': false

Result of running operator 'ValueEqualTo' on property 'AdminUser' and value 'false': false

Result of running operator 'VersionLessThan' on property 'VersionNT' and value '5.1.2': false

Result of running operator 'VersionEqualTo' on property 'VersionNT' and value '5.2.0': false

Result of running operator 'ValueEqualTo' on property 'ProcessorArchitecture' and value 'IA64': false

Result of checks for command 'DotNetFX35SP1\dotNetFx35setup.exe' is 'Install'

'.NET Framework 3.5 SP1' RunCheck result: Install Needed

EULA for components '.NET Framework 3.5 SP1' was accepted.

Copying files to temporary directory "C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\"

Downloading files to "C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\"

(2012-7-5 19:05:45) Downloading 'DotNetFX35SP1\dotNetFx35setup.exe' from 'http://go.microsoft.com/fwlink/?linkid=118076' to 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\'

Download completed at 2012-7-5 19:05:49

Verifying file integrity of C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe

WinVerifyTrust returned -2146762496

File not signed

Error: Setup has detected that the file 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe' has changed since it was initially published.

(2012-7-5 19:05:50) Downloading 'DotNetFX35SP1\dotNetFx35setup.exe' from 'http://go.microsoft.com/fwlink/?linkid=118076' to 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\'

Download completed at 2012-7-5 19:05:51

Verifying file integrity of C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe

WinVerifyTrust returned -2146762496

File not signed

Error: Setup has detected that the file 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe' has changed since it was initially published.

(2012-7-5 19:05:52) Downloading 'DotNetFX35SP1\dotNetFx35setup.exe' from 'http://go.microsoft.com/fwlink/?linkid=118076' to 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\'

Download completed at 2012-7-5 19:05:53

Verifying file integrity of C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe

WinVerifyTrust returned -2146762496

File not signed

Error: Setup has detected that the file 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe' has changed since it was initially published.

(2012-7-5 19:05:54) Downloading 'DotNetFX35SP1\dotNetFx35setup.exe' from 'http://go.microsoft.com/fwlink/?linkid=118076' to 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\'

Download completed at 2012-7-5 19:05:54

Verifying file integrity of C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe

WinVerifyTrust returned -2146762496

File not signed

Error: Setup has detected that the file 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe' has changed since it was initially published.

(2012-7-5 19:06:06) Downloading 'DotNetFX35SP1\dotNetFx35setup.exe' from 'http://go.microsoft.com/fwlink/?linkid=118076' to 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\'

Download completed at 2012-7-5 19:06:06

Verifying file integrity of C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe

WinVerifyTrust returned -2146762496

File not signed

Error: Setup has detected that the file 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe' has changed since it was initially published.

(2012-7-5 19:06:07) Downloading 'DotNetFX35SP1\dotNetFx35setup.exe' from 'http://go.microsoft.com/fwlink/?linkid=118076' to 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\'

Download completed at 2012-7-5 19:06:07

Verifying file integrity of C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe

WinVerifyTrust returned -2146762496

File not signed

Error: Setup has detected that the file 'C:\DOCUME~1\ADMINI~1\LOCALS~1\Temp\VSD285.tmp\DotNetFX35SP1\dotNetFx35setup.exe' has changed since it was initially published.