各位好:
我用到28004X的GPIO32管脚作为CANA-TX,但由于我是boot from flash 的,因此这个管脚需要上拉,由于没这样用过,所以问下大家,CAN-TX外部上拉可行么。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
也就是说您现在想实现:
1 boot from flash
2 GPIO32管脚作为CANA-TX
那您可以使用zero-boot pin mode,而不使用GPIO32
具体可以参考TRM的4.3.3.1 Zero Boot Mode Select Pins