芯片信号F280049,发波方式与F28377也比较像,现在采用PWM上下互补方式发波,PWMA输出经过上升沿和下降沿死区后输出ePWMxA和ePWMxB,预留一定死区,配置为HRPWM后,ePWMxA输出可以实现HRPWM,但是ePWMxB没有实现,再配置HRCNFG寄存器中的SWAPAB位和SELOUTB位均无法实现ePWMxA和ePWMxB后高精度完全互补,要么只有一路高精度,要么高精度互补后没有死区,请问应当如何解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
芯片信号F280049,发波方式与F28377也比较像,现在采用PWM上下互补方式发波,PWMA输出经过上升沿和下降沿死区后输出ePWMxA和ePWMxB,预留一定死区,配置为HRPWM后,ePWMxA输出可以实现HRPWM,但是ePWMxB没有实现,再配置HRCNFG寄存器中的SWAPAB位和SELOUTB位均无法实现ePWMxA和ePWMxB后高精度完全互补,要么只有一路高精度,要么高精度互补后没有死区,请问应当如何解决?
直接上TI的例程,例如Example_F2803x_HRPWM,60Hz主频下配置PWM为6MHz(PRD=10),然后CMPA按整数只能生成10%,20%...100^%占空比,通过计算CMPAHR可以得到连续可调占空比PWM,这就是HRPWM的效果:极大的提高了分辨率。