1.使用增量式光栅是否必须用到Index信号?motorware(v18)中有感算法(如lab12b)就没有使用Index信号
2.编码器计数max时对应的电角度应该是多少?是0.99吗?使用drv8301-69m kit,手转电机一圈,发现编码器计数max时电角度为0.63.使用motorware lab12b 电机每转一圈都会在编码器计数max->0过程中出现异常,有时启动也会出现异常。我感觉与编码器计数没有转换成正确的电角度有关
3.Ti有任何编码器使用,机械角度转换电角度的文档吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.使用增量式光栅是否必须用到Index信号?motorware(v18)中有感算法(如lab12b)就没有使用Index信号
2.编码器计数max时对应的电角度应该是多少?是0.99吗?使用drv8301-69m kit,手转电机一圈,发现编码器计数max时电角度为0.63.使用motorware lab12b 电机每转一圈都会在编码器计数max->0过程中出现异常,有时启动也会出现异常。我感觉与编码器计数没有转换成正确的电角度有关
3.Ti有任何编码器使用,机械角度转换电角度的文档吗?
1、需要接的,lab12b有用到z相信号用来零位置对齐的,代码如下:
// if we are forcing alignment, using the Rs Recalculation, align the eQEP angle with the rotor angle if((EST_getState(obj->estHandle) == EST_State_Rs) && (USER_MOTOR_TYPE == MOTOR_Type_Pm)) { ENC_setZeroOffset(encHandle, (uint32_t)(HAL_getQepPosnMaximum(halHandle) - HAL_getQepPosnCounts(halHandle))); }
2、你是观测的哪个变量值?
3、似乎没有这样的文档,instaSPIN的参考一般就用到lab手册和用户指导。
1.你贴的代码确实是为了编码器和转子的对齐,但并没有用Index信号。QEP_SETUP()里并没有为Index信号配置功能。曾在英文论坛看到过相关内容。
2.观测的enc_elec_angle,我想是以下代码的问题(ENC_SETUP中):
enc->mech_angle_gain = (_iq)((((uint32_t)1)<<24)/(4*num_enc_slots));
1/(4*num_enc_slots)放大2^24倍再取整,意味着mech_angle_gain缺失了精度,num_enc_slots越大,缺失精度越大以至于不能接受。